• ADDI9036 reference clock input

    Hello,

    I went through the documentation for this particular chip and I noticed that all parameters and connection examples are referred with a reference clock of 45MHz on pin C6 (CLI). Is it possible to feed 60MHz clock signal into pin CLI (C6)? Would…

  • Multiple camera interference in ADDI9036

    Hello,

    I have read the article about interference avoidance and cancellation in the following page https://www.analog.com/en/landing-pages/001/tof-story.html.

    I have few queries need to be clarified,

    1. Whether the interference reduction algorithm is…

  • RE: ADDI9036 Detailed Datasheet

    This issue would be better handled through the sales channel. Would it be possible for you to contact your local sales? 

  • NXP i.mx8 driver porting for ToF9036

    Hi Team,

    we are currently integrating some development project. This main goal is to connect the ADI 9036 TOF Module through mipi on the NXP i.mx8 mini target board.... In addition, the recommended development environment(released) by NXP is yocto, so if…

  • RE: No image from sensor: Failed to get frame from device

    Yes, I am powering the the interposer before the Raspberry Pi.

    And yes, I am using the latest SD card image (from here https://github.com/analogdevicesinc/aditof_sdk#supported-embedded-platforms, AD-FXTOF1-EBZ for Raspberry Pi 3,4).

    The whole output from…

  • RE: AD-96TOF1-EBZ Rev D Board with Jetson

    For Xavier NX I had to build also the SD card image based on NVIDIA's sample rootfs and their script. Now at least I can see the kernel probing the ADDI9036 sensor, which should be ok(?)

    [ 2.154288] addi9036 9-0064: probing addi9036 v4l2 sensor
    …

  • RE: AD-FXTOF1-EBZ with RPI4

    Hi,

    Should I modify dts to enable the camera?

    The unicam driver is loaded and the addi9036 seems not load correctly.

  • Help with dts on rpi compute module io board

    I have a Raspberry Pi Compute Module 4 installed on a Raspberry Pi Compute Module IO board. The IO board has 2 CSI connections. I wanted to bring up the ADDI9036 TOF dev kit on one of the  CSI ports. I have rebuilt the latest RPI kernel and also managed…

  • RE: Eeprom data corrupted?

    Hi,

    Thanks for your reply.


    I think it is not a hardware problem because when  I started the adi tof demo exemple
    with dmseg --follow command in background, and I have the following output:

    [ 6.467920] addi9036 0-0064: addi9036 detected at address 0x64
    .…