• addi7004

    We are trying to run the ADDI7004 with little success of just trying to power up the device and getting a LVDS TCLK out of the part.

    So far this is what we have done..............

    We follow the recommended power-up sequence found on page 34 to the letter…

  • ADDI7004

    Hi, 

    My customer is now facing component degrade issue on their board and need some information about the component reflow profile for ADDI7004. They need the information to study the root cause based on process perspective.

    I have requested the datasheet…

  • ADDI7004

    Hi there, 

    I just wonder how to read the date code on this product.

    I can’t found documentation for this guide.

     

    Do you have documentation that explain about this and the temperature profile about this device.

    Regards,

    Carmen.

  • ADDI7004 analog interface

    Hi,

    I'm looking for some help on how to interface a contact image sensor (CIS) to the ADDI7004.  Should I use an emitter follower between the output of the sensor and the analog input to the ADDI7004?  A reference design would be very helpful if anyone…

  • ADDI7004 TCLK usage

    When the ADDI7004 is used in double data port mode, I understand that the 8 differential outputs are used to transmit the data from the 4 channels. However I am a bit confused on the way to use the TCLK1 differential output clock in that mode.

    Is TCLK1…

  • ADDI7004

    Recently I studied the IC ADDI 7004 and I have some questions here :

    1. May I know what is the usage of horizontal counter and vertical counter? When do I need to supply the clock for VD and HD?

     

    2. I understand that SHD and SHP are important to achieve…

  • ADDI7004 speed

    I know ADDI7004 is spec for 72MHz. Is there a limit on how slow the part can operate? Interested in pixel rate of 15MHz per channel.

  • ADDI7004 speed

    I know ADDI7004 is spec for 72MHz. Is there a limit on how slow the part can operate? Interested in pixel rate of 15MHz per channel.

  • ADDI7004 Question

    Hi,

     

    I have a few questions about ADDI7004.

     

    Question 1

    Can we monitor DCR signal to know the SHP and SHD internal signal? How does DCR signal relate to SHP and SHD signal?

    I would like to know when SHP and SHD start to sampling the input signal…

  • ADDI7004 LVDS Pattern Generation.

    Hi,

    Currently I'm using ADDI7004 in our product development.

    We already fabricate the PCB for this board.

    1. I already follow the power-up/initialization sequence required to start-up the ADC IC.(Recommended Power Sequence Pg:34 ADDI7004 Datasheet…