Hi
We would like to know the horizontal axis of Figure-9.
20mSec/div?
Fig-10 to 13 were also missing those data.
Regards
moto
Great! I'm glad were both thinking the same thing. So here's how I would do it with the ADD5205:
NOTES:
1. Connect nSHDN to 1.5 - 6.0 V to enable the ADD5205. This is also where an oscillator would be connected for blinking.
2. Connect a…
Hi Jacky,
The ADP5587 is not the best solution. It's pulldown pins are only spec'd at 1mA. And the pins are only rated to 4V (max). This would be a problem if one of the LEDs was off--then the pin would be pulled up to almost 9V.
Instead, we…
最新解决方案已上线,点击:http://h.analog.com/CN-VC-ANALYZER-ff?ADICID=SOME_CN_P114971 下载完整文档
体外化学分析仪的典型架构
生命科学与医疗仪器仪表包括各种不同的系统,比如体外化学 分析仪、流式细胞分析仪、输液泵、透析设备、呼吸器、导管 等设备。体外化学分析仪利用许多电化学和光学技术来分析血 液、尿液、脑脊髓液和其他生物学样本。其中使用最广泛的技 术是光学测量,实例包括比色、吸收、光谱测定和荧光检测方 法。可通过这些方式测量体液中的抗原…