• RE: ADCMP605 hysteresis input

    Hi, I just noticed this post was a few years ago but was the correct answer to add a 70K resistor or 7K resistor to grounds as I am in the process of evaluating the comparator 

  • ADCMP605 Shutdown State

    Hi

     I have a couple of question.

     

    ADCMP605 have shutdown pin(PIN#7).

    When the part is in shutdown,

    Q1)Are the outputs(Q=PIN#12, Q^=PIN#10) placed in a “high impedance” state?

    If so, Can you recomend pull up register value?

    Q2)Can the inputs…

  • Does ADCMP605 LVDS Output Stage include 100 ohm termination?

    Does the ADCMP605 LVDS Output Stage include the 100 ohm termination?

  • ADCMP605 input model

    Hello

    I would like to find out if there is a basic model of the VP/VN input pins for the ADCMP605 comparator? I would like to simulate the loading of a driver connected to multiple ADCM605 devices in parallel.

    What effect does the LE/HYS pin have on…

  • ADCMP605


    关于ADCMP605器件的LVDS输入、输出匹配电阻的问题:对于这样的高速比较器,LVDS布局布线的要求,以及对源端和输出端电阻匹配的要求如何?可以直接按数据手册上的方式接么?

  • ADCMP605 EVM user guide

    Hello EZ, 

    Would you advise the download link of the user guide of ADCMP605 EVM?

    I purchased this board, but I want to have its schematic and connection guide. 

  • ADCMP605 Latching

    I have the ADCMP605 comparator and I want to know how to latch it to stay high for 10ns. Any ideas? 

    Thanks,

    Suhani

  • RE: Regard to the design of ADCMP605

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: I sincerely need some help with the ADCMP605 application? DUTY CYCLE?

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • ADCMP605这个高速比较器的电源VEE是否一定要接地?

    请问ADCMP605这个高速比较器的电源VEE是否一定要接地?如果可以接负电源,那么输入信号可以是负信号脉冲吗?