• RE: adcmp601 spice simulation

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: Voltage of ADCMP601 when inputs were left floating

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: Cannot run the ADCMP601 simulation file on OrCAD 10.5

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: ADCMP601 hysteresis setting resistance(Rhys) vs dispersion of hysteresis threshold

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • To adjust a hysteresis threshold of ADCMP601

    I'm looking for the way to adjust a hysteresis threshold of ADCMP601.
    Advice, please.

    I paid attention to ADCMP601 for my product.
    I'd like to adjust a hysteresis threshold of ADPCMP601 to the specific  value (for example, 30 mV ± 5 mV).
    How should…

  • 求助:关于ADCMP601比较器SPICE文件的使用

    您好:

    请问该比较器(ADCMP601)可否用ADS做仿真?若不可以,那什么软件可以仿这款比较器?

    谢谢您的回复。

  • ADCMP601这个比较器对于输入信号的功率范围要求是多少?

    ADCMP601这个比较器对于输入信号的功率范围要求是多少?官网上数据手册并没有一个明确的说明,要用这个做一个测200MHz频率的频率计,大神们指导一下~

  • 求助,关于ADCMP601比较器SPICE模型仿真的问题

    我用multisim13.0 进行仿真,在创建元器件的第5步,加载从官网上下载的cir文件时遇到问题,提示如下:

    因为这个错误导致无法“下一步”。换用multisim11倒是可以创建成功,但是仿真时直接报错,而且提示了一大堆“max”、“min”未定义。怀疑是cir文件本身的问题,求解答,谢谢!!

  • ADCMP609 pspice model

    I am looking for pspice model for these comparators: ADCMP609 & ADCMP602.

     

    Unfortunately there is no pspice model available for ADCMP609 at the moment.
    There is a model for the ADCMP601. However, the ADCMP600,601,602 are all the
  • RE: ADCMP600 SPICE Model

    * ADCMP601 SPICE Macro-model
    *   06/26 Draft
    * LPS APPS Engineering
    *
    * This is not the final version of ADCMP601 Spice model
    *
    * This model was created based on the HSPICE version of ADCMP601 by JAV on 6/25/2018
    * The ADCMP601 HSPICE model was modified…