Hi!
Figure 22 in the ADCMP600 data sheet shows a "Self-Biased 50% Slicer" circuit. Is this circuit suitable for converting a 10 MHZ Sine
to Square Wave.
Input Signal can range from 0 dBm (0.6V pk-pk) to 15 dBm (3.5 V pk-pk)...Input signal…
Hi!
Figure 22 in the ADCMP600 data sheet shows a "Self-Biased 50% Slicer" circuit. Is this circuit suitable for converting a 10 MHZ Sine
to Square Wave.
Input Signal can range from 0 dBm (0.6V pk-pk) to 15 dBm (3.5 V pk-pk)...Input signal…
Hello, I have been simulating and have built prototypes of the circuit described in TI App Note SLAU508: https://www.ti.com/lit/ug/slau508/slau508.pdf. I implemented this app note using LTC6268 and ADCMP600.
The circuit works well and is used to drive…
I have the attached circuit prototyped using ADCMP600 and LTC6268:
VTRI:
V_R14 (output of error amp):
The problem is the PWM output has some strange non-monotonicity points both in rising edge and falling edge:
Can anyone explain why these "jagged…
Hi William,
ADCMP600 might not suit your requirement in terms of the input voltage you require which is +/-2.5Vpp, because it can only operate with +2.5 to +5.5V positive supply and GND supply. With that, the input range allowed is minimum of -0.5V.
…Dear Team,
I want to make current control via MOSFET based on LTC1968. The load will be full wave rectified sinusoidal ( not filtered ) and frequency will be max 400hz.
My design is in the attachement.
Hi,
I configured the parametric selection table of ADI comparators based on your requirements. Kindly check this link
and select among the parts from the configured table which will best suit your application.
On your second point, usually comparators…
Hi Chen,
I am attaching the schematic of the adcmp601 evaluation board, the operation is straight forward it uses SMA for the input connection and banana plug for the supply.
Regards,
Joven
可以看一下ADCMP600 ADMCP601 ADMCP602
资料如下
http://www.analog.com/cn/products/linear-products/comparators/adcmp601.html
Hi,
Could you please suggest me a comparator which can driver the 50ohm load. Currently we have used ADCMP600 in our design.
For any clarification feel free to ask me.
Regards
Anand M