• ADCMP580/ADCMP581/ADCMP582 input nose model

    Can you please provide input noise models for ADCMP580/ADCMP581/ADCMP582?

     

    We do not have any models for available for the ADCMP580/ADCMP581/ADCMP582.
    However, the datasheet does contain typical jitter numbers which  may help.
  • ADCMP582 Vtt

    HI

    i am trying to evaluate THE ADCMP582 on ADI evaluation board.

    i am trying to disable the LE feature,  so i connect nLE to the Vtt (green) and LE pin to Vcco with a 750Ohm resistor. i am getting 0.06V diff voltage on the LE pins, so i think it's should…

  • ADCMP582

    Hello,

    I am looking into the adcmp582 for a high speed triggering circuit.  In reading the datasheet I've run across multiple specs regarding dispersion.  What does this mean?  For example, Slew rate dispersion or pulse width dispersion?  Is this just…

  • RE: ADCMP582 Input termination resistors maximum dissipation

    Hi,

    Sorry for the very delayed response.

    I checked the design schematics of ADCMP582 but I need to look internally for someone or document regarding the power dissipation spec or capability of the internal resistor model/type used  in the input termination…

  • RE: ADCMP582 PECL

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: ADCMP582 Comparator: Disable Latch Feature.

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • About processing method of Exposed pad of ADCMP582

    Hi,

    I would like to use ADCMP582.

    So, I have a question. Please help me.


    Question:
    Please tell me about correct handling of Exposed pad.

    The following statement is on page 8 of data sheet.


    Although the description about Exposed pad is only in this…

  • ADCMP582 Oscillating

    I've got a design with an ADCMP582, and the output oscillates whenever the differential input voltage gets under about 50mV.  I saw the note in the datasheet about keeping the slew rate above 50V/us, but that can't be what's going on here; if you can…

  • RE: Input voltage of absolute maximum ratings for ADCMP580, ADCMP581 and ADCMP582

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • ADCMP582 IBIS model import to Advance Design System

    I want to use ADCMP582 IBIS model on Advance Design System but I don't know how to import IBIS model to ADS. I would be pleased if there is anyone who knows how to do it.