• ADCMP581 input capacitance

    What is the value of the ADCMP581 analog input capacitance? I did not find in the data sheet.

  • ADCMP580/ADCMP581/ADCMP582 input nose model

    Can you please provide input noise models for ADCMP580/ADCMP581/ADCMP582?

     

    We do not have any models for available for the ADCMP580/ADCMP581/ADCMP582.
    However, the datasheet does contain typical jitter numbers which  may help.
  • RE: ADCMP581手册参数请教

    This question has been closed by the EZ team and is assumed answered.
  • RE: What's your recommend ECL Receiver/Driverfor Voltage Comparators ADCMP581?

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • ADCMP581 Power Consumption

    I just wanted to ask the total power consumed by ADCMP581.

    As per data-sheet:

    ADCMP581 (NECL)
    Positive Supply Current: IVCCI: VCCI = 5.0 V, 50 Ω to −2 V: 6 mA
    Negative Supply Current: IVEE: VEE = −5.0 V, 50 Ω to −2 V: −25 mA
    Power Dissipation: PD: 50 Ω to −2 V: 

  • RE: Input voltage of absolute maximum ratings for ADCMP580, ADCMP581 and ADCMP582

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: ADCMP580 Latch Enable/Disable

    HI Fabian,

    The datasheet description is consistent from table 5 and Using/Disabling the latch feature section (page 12).

    On table 5, it states that in order to disable the latch feature the following configuration must be used:

    LEB = Low
    LE   = High

    On…

  • RE: What is the random jitter specification of ADCMP566 dual high speed comparator?

    Hi Joshua,

    The ADPCMP566 is an old part and hasn't undergone the same evaluation as ADCMP581.

    We don't have enough test data to provide regarding the random jitter specification. We can however do some evaluation for a typical specification but…

  • RE: Questions for your ATE device ADCMP580

    Hi, Kaos.

    ADCMP580, ADCMP581 and ADCMP582 have the same datasheet which you can find here. The main difference of these three comparators is the output driver wherein ADCMP580 is CML, ADCMP581is NECL and ADCMP582 is PECL.

    But since you need the tr/tf…