Hello,
Can Analog Devices provide a full characterization of Vp and Vn analog input (ADCMP580) in terms of S-Parameters up to 18GHz?
Thanks in advance
Best Regards
I would like to drive an ac-coupled differential 50 Ohm load with the ADCMP580 (or 582). The load is in fact the REF/NREF input of the HMC4069 (with DC block).
What is the best way to terminate the ADCMP580 outputs and to connect the REF/NREF input of…
我想问一下,ADCMP580为什么没有SPICE模型?还是忘了给链接了(虽然这种可能性很小),而且很多快速比较器都没有给出SPICE模型是什么原因?
电压比较器ADCMP580,输入端一个接正弦信号,一个接直流电压信号,现在直流信号接0V,正弦信号幅度峰峰值500mV,频率低于50MHz,输出信号为占空比50%的方波,但是大于50MHz后,输出信号就不是方波了,频率越高,信号就越接近正弦波,请问器件本身就是这样还是有其他问题?
I have used the Analog evaluation board for ADCMP580 and I'm very happy with I would like to reproduce such board in a small factor form
I need to know what is the substrate used in the eval board and the brand of the decoupling capacitor
Hello,
One of my customer would like to use ADCMP580 in his new design.
He want to know the input capacitance for the Vp and Vn terminals.
The capacitance variation depending on input voltage is also helpful, if available.
He will use the capacitance…
The spec is about VCCI=5V and VEE=-5V. It seems the ADCMP580 could work with single power supply, but there is no parameters about it.