• ADCLK950 Vcc range specification

    Hi,

    The ADCLK925  has specifications for Vcc= 2.5V, 3.3V, but large device as ADCLK950 is only for Vcc= 3.3V+-10%. Is it possible to use ADCLK950 with Vcc= 2.5V?

  • ADCLK950 specifications for low frequencies

    Hi,

    For one of our project, we need to design a very low phase noise distribution links to broadcast a 38.4MHz LVPECL clock (50% duty) to an undefined number of devices (1 to 512 with a cascaded buffer clock tree architecture).
    The ADCLK950 seems to be…

  • Using the ADCLK950 for a pulsed application / random pulse patterns.

    Hello everybody,

    I recently started gathering information for a new project. I need to have a pulsed trigger signal transmitted to 10 ICs with very small jitter.

    For example 100 pulses with 10ns length and 50 ns gaps in between. And that pattern is repeated…

  • Phase noise and Jitter for a high speed fanout chip

    Hi guys,

    We are designing low phase noise distribution links.

    The question raises on how does the additive phase noise of a fanout chip varies with input frequency changes.

    If considering PLLs, DDSes or Dividers, we know the output phase noise has…

  • RE: Low-jitter clock mux

    Hi Donald,

    The ADCLK950 will fan out 1 of 2 reference inputs controlled by an external pin.  How many outputs do you need?

    http://www.analog.com/en/clock-and-timing/clock-generation-and-distribution/adclk950/products/product.html

    Additive broadband…

  • TAGS LIST: Clock and Timing

    LTC6953
    LTC6955
    LTC6957-1
    HMC6832
    HMC7043
    LTC6950
    LTC6954
    HMC987
    AD9576
    AD9508
    HMC1035
    HMC988
    HMC1033
    HMC1034
    HMC1032
    HMC1031
    ADN4670
    ADCLK944
    ADCLK950
    ADCLK948
    ADCLK846
    ADCLK954
    ADCLK946
    ADCLK854
    AD…
  • 3月重点推荐——民用雷达解决方案,是你的菜么?

    雷达广泛用于民用应用,从执法部门实施的汽车系统和速度监控到空中交通管制、天气和海上监控。雷达发射无线电波,然后通过其路径中的物体反射。雷达接收机处理这些反射波以确定物体的范围、角度或速度。例如,海上雷达可测量船舶方位和距离以防碰撞并进行船舶导航。在港口或海湾处,船舶交通服务雷达系统用于监控和调节繁忙水域中的船舶运动。配合飞机应答机系统一起使用的类似民用空中交通管制雷达确定相似特性,以确保飞机之间保持安全距离并协调飞行路径。

    主要挑战和系统设计考虑

    远程监控雷达,如空中交通管制、天气和海上雷达…

  • 【在线研讨会回顾】高速电路设计之频率合成和时钟产生

    在设计团队不断精益的今天,工程师不仅需要深厚的技术积淀,而且必须能够跨专业设计。从模拟到数字,从硬件电路到软件,样样精通,无所不能。ADI2013在线设计峰会,旨在帮助您在一个日益复杂、压力巨大的世界里简化设计。


    查看ADI 2013在线设计峰会相关研讨会视频及资料,请点击http://ezchina.analog.com/message/9778

    研讨会上的演讲稿,请见附件

    Attachments: