• Clarify of the ADCLK854 with single-ended input

    In the datasheet, "AC-Coupled input applications", it says:

    The ADCLK854 offers two options for ac coupling. The first option requires no external components (excluding the dc blocking capacitor), it allows the user to simply couple the reference…

  • ADCLK854 input sensitivity

    Hi,

    I would like to check if ADCLK854 can work with 100mV input.

    According to the datasheet, ADCLK854 input sensitivity is 150mV typical, but what is the possible minimum input for the ADCLK854.

    Thanks.

  • ADF4360, ADCLK854, Thermal Resistance Values Needed

    Hi,

    I am interested in the thermal resistances of the following parts. Specifically I am interested in the junction-to-case and junction-to-board thermal resistances. 

    ADF4360-5BCP

    ADF4360-4BCP

    ADCLK854BCPZ

    Thanks, 

    Sadab Bahar

  • ADCLK854 lacking output

    Hi, eveyone.

    I'm evaluating ADCLK854 evaluation board.
    I found a lacking output. I don't know it was caused by measurement issue or others.

    Hear is the detail.

    We input "burst clock" to this device.
    It can be seem at "first burst clock…

  • RE: AC coupling capacitor position relative to termination resistor of ADCLK854 input

    Hi,

     I believe here is important to follow the recommendations of the source generating the ADCLK854 clock input.

    Petre

  • ADCLK854 Clock buffer phase noise

    Hi

    I want to estimate 40MHz phase noise of ADCLK854 from datasheet fig.12.  I found a similar discussion in engineer zone.

    https://ez.analog.com/message/28494#28494

    My first question.

    If input slew rate was not an issue at 40MHz and phase noise is…

  • ADCLK854 Eval board LVDS swing measurement

    Hi,

           Our lab recently purchased ADCLK854 eval board and we are testing the LVDS outputs and observed that the outputs wing does not go to 700mV full swing. The output signals are ac coupled so I guess it doesn't go full swing if SMA cable is connected…

  • ADCLK854 250MHz phase noise plot for LVDS output

    Hello,

    Does a 250MHz phase noise plot or table for a LVDS output exist for the ADCLK854?  I see the datasheet includes a table and plot for 1GHz.

    Thanks.

  • RE: LVDS clock Buffer - output swing (AC coupling)

    Hi Veera,

    I can only speak on behalf of the ADCLK854 but if I am understanding correctly, the ADI part is labeled "LVDS1" in your original picture.

    This seems like the IBIS model is accurate with respect to the expected operation.  All of our…

  • RE: XXXXXXXXXX Output Clock Level Compatability

    We recommend the ADCLK854 for what you are trying to do.  If you wish to ask about that product, we can answer.  The part # you posted about is a competitors device; we have no support to provide you on that product.