FAQ
Hi,
In AD-FMCOMMS5-EBZ design, I saw that ADCLK846's input oscilator (RXO3225M) is not availaible to buy in digikey and mouser. Thats why I looked for another oscilator for ADCLK846. but I could not proper oscilator in Vpp =1.8V(input level of ADCLK846…
Hello
Actually I have some AD9851 DDS ICs in my circuit like the below:
so I need a CMOS clock distributor to feed them simultaneously.
the supply voltage for AD9851 is +5V bcoz in this condition the maximum output frequency can be achieved as following…
When using AD9953 in multiple synchronize mode, adclk846 is used as single ended cmos input / output mode for distribution of SYNC_CLK.
1. Pins not used in the input are supposed to be processed to ground using CAP. How to terminate the unused pins in…
Hi,
can I use a 52 MHz TCXO, like the LFTCXO073006, as AC-coupled input clock for the ADCLK846?
Moreover, I was wondering if it's possible to shut down some outputs by disconnecting the closest Vs pin.
Thanks
Regards
Hi ~.
I am trying to find appropriate handling guide for unused output channels of ADCLK846 especially in CMOS channel as attached schematics.. do we have guideline or don't care?
Regards,
Angela