• RE: ADAV803 problems

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: ADAV803 Internal Registers Problems

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: ADAV803 Question Please help me!

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: Disabling CPLD on EVAL-ADAV803/EVAL-ADAV801

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • ADAV803 SRC clock question

    Table 2 on page 4 of the ADAV803 datasheet lists SRS MCLK Min = 138 x Fsmax but the text on page 21 states "The SRC master clock is expected to be equal to 256 times the output sample rate."   These appear to be conflicting statements..  Please…

  • ADAV803 technical questions

    Hello

    I have some technical questions regarding ADAV803.

    According to the application note AN-910 it should be used since a problem could occur when the S/PDIF connector is disconnected and reconnected several times successively. The problem can also…

  • What is the "rate register" on the ADAV803 and how do you use it?

    I'm having trouble getting the SRC to work properly in the ADAV803.  What is the "rate register" and how do you use it?

  • Does ADAV803 have the capability to decode multichannel S/PDIF and output TDM8 serial data?

    Hi

    I am using ADAU1761, and I want to input audio from S/PDIF. I saw CN-0219, and I'm using it as a reference, but I can not find any information regarding support for multichannel audio. I want to know if ADAV803 can decode multichannel or surround…

  • ADAV80x digital output with transformer

    Hi,

    For a new design I'm planning to use the ADAV803. I also need the DIR and DIT functionality, but using AES3 compatible in and outputs.

    Is the ADAV80x capable of directly driving the required transformer? Or should I buffer the signal using a…

  • 2010-05-15 09:23:31     i2c driver in kernel

    2010-05-15 09:23:31     i2c driver in kernel

    Appalayagari Sreedhar (INDIA)

    Message: 89433   

    Hi,

    I am working with a Blackfin BF533 based custom board 2009R1-RC1 distribution. audio codec is i2c interfaded. 

    i2c emulation using the PF0 and PF1 pins.…