• RE: Is PLL filter always needed in ADAU1978?

    Hi Dave, yes, the answer is quite late and we already discovered that PLL is needed.

    We have had additional trouble with phase synchronisation of two ADAU feeded with the same TDM signal. Thanks to the support of your colleague Salvatore Napolitano (Italy…

  • ADAU1978 Digital DC high-pass filter

    Hello,

    I'm using ADAU1978, can you please clarify the use of the digital DC high pass filter configured in register 0x1A bits 0-3?

    Also, how is it working with enabling DC calibration (in register 0x0E bit0) and DC subtraction configuration?

    Regards…

  • ADAU1978 clipping status

    Hi,

    Regarding the ADC CLIPPING STATUS REGISTER - how often does this register update? Is it set when clipping is detected and cleared when read? does it update every time interval? 

    If clipping is detected - should I see a value of 0x7FFFFF on the output…

  • RE: ADAU1978 at 192 KHz: noise at high frequencies

    Hi, 

    Apologies for missing this item. I am not sure if it still relevant to you that this question will be answered, However, we are clearing up some open items in our community and ensure that any query is located on its proper community as others who have…

  • ADAU1977/ADAU1978/ADAU1979 PLL and Clock settings, when sampling rate is lower than 32kHz

    Hi,

    Please let me ask how to configure PLL and Clock when the sampling rate is lower than 32kHz.

    For example, when sampling rate is 16kHz on the ADAU1978,
    how can we decide SAI_CTRL0.FS and PLL_CONTROL.MCS values, and MCLKIN frequency?

    Depending on the sampling…

  • ADAU1978 TDM problem

    Hello,

    my ADC sends wrong datas on TDM, this is an example :

    The BCLK and LRCLK signals are sent by a FPGA, they don't seem too bad (probed with a 2GHz active probe) :

    LRCLK is sampled by the ADC on rising edge, here are the ADC registers :

     ADC…

  • RE: ADAU1978 configuration

    Hi Dave,

    Sorry for delayed response. I am trying to store I2S data by simply opening a file with the .wav extension. Then the microcontroller that i am using has i2s peripheral on it,so i simply do a i2s receive and then try to store the data which is…

  • Questions about ADAU1978 in SA mode

    Hello I want to use the ADAU1978 in SA mode.

    For this I connect:

    1. SA_MODE to IOVDD (for standalone Hardware mode) .

    2. ADDR0 to GND (for I2S mode)

    3. ADDR1 to IOVDD (Slave mode). SigmaDSP processor will supply LRCLK and BCLK. PLL filter will be configured…