• Adau1966

    I have a digital audio mixer device that uses the adau1966 ic as its output dac, and there is damage to the output, no sound comes out. and i have replaced the new adau1966 ic. do I directly install the ic or do I need to set the registers to match the…

  • Adau1966

    have a digital audio mixer device that uses the adau1966 ic as its output dac, and there is damage to the output, no sound comes out. and i have replaced the new adau1966 ic. do I directly install the ic or do I need to set the registers to match the…

  • ADAU1966 maximum load current

    How much current can I draw from the analog outputs? The datasheet does not
    give values for the maximum recommended currents.

     

    We do not specify a maximum amount of AC current that the part can supply,
    rather we say that the part should be driving…

  • RE: ADAU1966 software question

    Hi Dave:

          Sorry for the delay in answering. 

           When the customer started ADAU1452, the child process started ADAU1966, so the clock was not allocated, which led to this problem. Now it has been solved. Thank you for reminding me

    terry yuan

    Thanks!

  • How to connect unused SDATA inputs on ADAU1966?

    How should I connect unused SDATA inputs on ADAU1966?

     

    You should treat SDATA inputs on ADAU1966 the same as any unused logic/digital
    inputs, we recommend tying them to GND.

  • ADAU1966: If using a direct MCLK can I leave LF and PLLVDD pins disconnected?

    Regarding the PLL of ADAU1966, I intend to use a 48kHz FS with a
    24.576MHz master clock. I can provide all the clocks to the ADAU1966.
    Can I completely disable the internal PLL or do I still need to connect the
    PLLVDD and LF circuits ?

     

    As you…

  • ADAU1966 Communication over TDM bus

    Hello everyone!

    It's the first time that I am using ADAU1966, and it looks like I can't make it work! 

    More specifically I am looking at the  Communication over TDM bus, I am sending signals but ADAU1966 is not responding to generate anything.

    Is…

  • ADAU1966

    Hi, 

    We are trying to use this DAC to generate constant voltages to control some test equipment (so not fast changing audio, DAC was chosen by our customer). This is having to be driven by a PIC32MX in TDM 16 mode. However as the PIC32 does not support…

  • EVAL-ADAU1966 Data Input by SPDIF Reciever

    Hello,

    I am planning to purchase the EVAL-ADAU1966 for a project, but there are some issues I would like to be clarified.

    The 12 channel audio input (192KBps 16bit) need approx. 4.5 MB/s bandwidth. How the evaluation board can input the regarded multichannel…