• RE: ADAU1962 Popping noise after Power-ON

    Hello Ramesh,

    Sorry for the missed reply. The EZKit is using an ADAU1962A only using the DACP outputs single ended. When the power up bit is engaged the DAC output come up to the common mode output voltage. If the output were to be used differentially…

  • ADAU1962 带A和不带A的2种后缀有什么区别?

    您好,我想请问一下ADAU1962AWBSTZ和ADAU1962WBSTZ,带A和不带A的这2种后缀有什么区别?是否可以通用? 麻烦请尽快回复,谢谢!

  • ADAU1962 BCLK but no LRCLK.

    Hello, I need some help please.

    I have an ADAU1962 operating in standalone, master mode that is outputting BCLK but not LRCLK. LRCLK pin is stuck at 0v, it's not shorted to ground. Before I replace the part I thought it smart to have someone verify my…

  • ADAU144x and ADAU1962 TDM8 serial output configuration.

    Hello, I'm having troubles setting the serial ports to TDM8, I've previously worked with 2 channel DACs and SigmaDSP but this has me stumped.

    ADAU1962 is master in standalone mode, TDM8 pulse.

    ADAU1446 is slave. I'm using clock domain 3.

  • RE: ADAU1978 and ADAU1962 LRCLK input jitter

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: Can't Run the adau1962 DAC on the ARM

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • Are ADAU1962 & ADAU1978 available in SigmaStudio?

    Dear Sir,

    I can't find ADAU1962 & ADAU1978 in SigmaStudio (Ver 3.13).

    Can you please kindly advise how to find these two component or is any library that I can import to SigmaStudio? 

    Thanks very much !

    Henry

  • RE: configuring the ADAU1962 to tdm8

    Hello,

    I am going back through old posts we missed. Sorry about that. Did you work out this issue?

    Dave T

  • RE: I2S输入多通道输出

    你可以用AD1938,这是4进8出的CODEC。

    或者你用ADAU1962,这是12出的DAC。

  • RE: Power-On Self Test (POST) on ADSP-21569 EZ-Board

    In the SPT_GBL_Audio_Passthrough_TDM and Audio_Loopback_TDM examples, there is a problem in configuring the ADAU1979 and ADAU1962 registers

    In ADAU1962, the value of the DAC_CTRL0 register is 0x18.

    In ADAU1979, the value of the SAI_CTRL0 register is…