ADI的专家你们好,
我在做ADAU1450的案子,发现这个跟1701设置有很大区别,现在主要碰到几个问题,ADC音量不能工作,ADC调节EQ也不行,还有ADAU1450不能用效果REVERB,显示DM1超了,能不能把REVERB设置在DM1,其它的都设置在DM0?另外还要做一个信号灯,用1450的IO口输出,设置灵敏度,比如检测到-60dB以上信号IO输出高,用于点亮LED,能给我个设置好的图吗?不胜感激!
盼回复!
ADI的专家你们好,
我在做ADAU1450的案子,发现这个跟1701设置有很大区别,现在主要碰到几个问题,ADC音量不能工作,ADC调节EQ也不行,还有ADAU1450不能用效果REVERB,显示DM1超了,能不能把REVERB设置在DM1,其它的都设置在DM0?另外还要做一个信号灯,用1450的IO口输出,设置灵敏度,比如检测到-60dB以上信号IO输出高,用于点亮LED,能给我个设置好的图吗?不胜感激!
盼回复!
I did a volume control test in the ADAU1450 and found no way to control the volume output (only no output and 3dB 2 results)
Hi,
Are there any know issues with the routing matrix of the ADAU1450 module?
The reason for this questions:
Actual configuration:
ADAU1450 and sigma studio 3.11.2.
There are no output signals at S_DATA_OUT 0..3.
LRCLK, BCK signals seem to…
The recently released ADAU1452 is an available target device in Sigma Studio 3.10 beta. This SS version also includes ADAU1450 and 1451 as possible target devices. However, I don't see any information on the latter two part numbers on the ADI website…
We have a product based on the ADAU1701 and a microcontroller. The microcontroller uses SPI to load the DSP program and update parameters on the fly using hardware safeload writes.
We are considering migrating to the ADAU1450, and we are wondering what…
In my project I used the ADAU1450 to self-boot. I‘m having trouble with popping noise when I switched EQ.
I have used DC-BLOCKING in my design. I also tried to mute before switching data, but these effects are not ideal.
I would be very grateful…
我是新手,我有一个单独ADAU1450,没有MCU。
~但我发现我没法把程序烧录进去(SPI连接,在线编译时SigmaStudio MODE为红灯),最终我需要让测试版自启动
~还有如何修改为使用I2C?
~USBI连接MISO、SCLK、SS、GND?
非常感谢!
Hi,
Can someone suggest me some production programming tools for
ADAU1450?
TKS
Best regards
Patrizio
We have developed an ADAU1450 board with AA1024 EEProm, following the scheme of the evaluation board.
Now we want to start the production, but the programming process of the EEProm through DSP takes a lot of time.
I've tried to use the WinE2PromLoader…
Hi All,
I am using a Adau1450 with three I²S inputs and three I²S outputs. Output0 is master of BCLK and LRCLK and should generate a LRCLK of 93750Hz. For two channels, BCLK should be 93750*32*2 = 6Mhz
The DSP is clocked on MCLK with 24.0MHz. I attached…