• ADAU1446 clock domain clarification

    Am planning to use the ADAU1446 to receive digital audio in a variety of formats, possibly process it with Sigma Studio functions, then spit it out in different formats. At the basic level, I'm using it as a pass through format converter. All inputs and…

  • RE: ADAU1446 gpio pins

    Hello rwalborn,

    No, the DSP does not need a program for the slave comms port to be able to write to registers. So you can change pins to GPIO registers without the core running a DSP program. 

    Yes, the power up state is set to input. 

    Dave T

  • Best platform for Guitar Effects devices - Questions relating to ADAU1446?

    Hi everyone

    I'm wanting to develop a platform for DSP guitar effects for use in a commercial product, and having looked at what others are using I've seen that the ADAU 1446 is used in the some of the products I like the most.

    I'm a start-up business…

  • ADAU1446

    there are four audio inputs, which algorithm shall i use to change 4 into 7.1. 

  • RE: Wiring up the ADAU1446

    This question has been closed by the EZ team and is assumed answered.
  • RE: ADAU1446 Max SPI speed

    This question has been closed by the EZ team and is assumed answered.
  • RE: AVC block on ADAU1446

    This question has been closed by the EZ team and is assumed answered.
  • RE: ADAU1446 serial slave clock input

    This question has been closed by the EZ team and is assumed answered.
  • adau1446 input / output continuity

    Hi, I have

    TDM2 16bit I2S selected on input 4

    TD8 16bit I2S selected for output 4

    on the adau1446. I'm switching clock domain 4 SD pin from input to output mode and switching the input/output on/off depending if I'm recording or playing back audio…

  • RE: ADAU1446 and AD1938/9 clock and programming

    This question has been closed by the EZ team and is assumed answered.