Hi,
Might I know if ADI have any ADAU1401A manual besides datasheet?
We find ADAU1401A initialization procedure is not in detail. Might I know if ADI has the timing diagram for setup sequencing and power up time for ADAU1401A?
We shall follow the guide…
Dear support team,
I have a question about power line.
ADAU1401A makes core voltate(1.8V) from 3.3V.
Q1:
If 3.3V power line goes down to arround 2.5V, is core voltage gone down? or does it remain 1.8V?
Q2:
At Q1 situation, if core voltage remains…
Hello, Dave-san
Thank you for your answer.
I got it.
Regards, TomY
Hello TomY,
I will add to what op-electronics mentioned.
The output is specified as a typical then you need to look at the gain error specification which is +/- 10%. Keep in mind that this is over all temperatures and skews so you will not see this much…
Could you tell me about aoutput impedance of DAC in ADAU1401A,please?
Best regards,
Takehiro Yabune
SigmaStudio(3.6.2 latest version) wrote 0x00,0x08 data to 0x081D register.
But datasheet said that this register is reserved.
Should we write it to this address or should not?
Is it possible to connect a microphone to ADC of ADAU1401A?
Since there is not MICBIAS, etc. on ADAU1401A, so I believe that it is difficult
Do you know any solution to connect a microphone to ADAU1401A?
Best regards, TomY
I confused about these descriptions below:
Datasheet P.17
RECOMMENDED PROGRAM/PARAMETER LOADING PROCEDURE
So I have a design where we're pulling audio sources into ADC0 and ADC1, Additionally, I've two channels of I2S connected to SDATA_IN0. The DSP is the master, and has its LRCLK and BCLK on MP10 and 11 tied back to the LRCLK and BCLK inputs on…
Hello all,
I am considering the possibility of using the ADAU1401A in my project.
I wish to use several external codecs with I2S bus. the codecs are in slave mode.I've noticed the ADAU1401A serial input port works only in slave mode, while the output…