• RE: Problem with ADAU1361 in slave mode

    The MCLK must be synchronous to any audio streams you connect to an ADAU1361.  This device has no ASRC deal with asynchronous data.  Look at getting a standalone ASRC device or utilize a codec with ASRC built in(ADAU1772 or ADAU1373).

  • Audio 180 degree out of phase

    Hello All,

    I have situation where audio is 180 degree out of phase, because of which it doesnt work on some websites.

    I am using ADAU1373 codec, I have inputs configured as a differential, I capture in mono mode, so Input 1 goes to left ADC and right…

  • ALC analog PGA

    Hello,

    I have been working on ADAU1373 codec, I have ALC working in digital PGA mode, but the problem is there some issue with some of the players (video uploaded on facebook) not able to play the audio properly (VLC, WMP.. can play it fine).

    If I disable…

  • 2011-06-20 03:31:53     WM8978 codec in alsa driver model

    2011-06-20 03:31:53     WM8978 codec in alsa driver model

    ThangarJ P (INDIA)

    Message: 101469   

    Hi All,

    we are working in BF527 based custom board and 2010RC1-RC4 distribution.

    is it possible to test the WM8978 codec using the alsa driver model?

    please…

  • RE: Analog audio and multiple I2S audio mixing.

    Hello Elango,

    Since you have two I2S lines it makes this more complicated. We have several small DSP products that can take an analog signal and an I2S/TDM signals and sum them in a small DSP and then send it out to an on-chip DAC and out of the serial…

  • Unhandled exception in Sigma Studio 3.5

    Hi all,

    I get an "unhandled exeption" everytime when I want to connect a Hierarchical input to a T connection. I did this many times before in the project but now it doesn't seem to work ... I already restarted a number of times, went back to a previous…

  • TAGS LIST: Audio

    AD8024
    AD8509
    AD8511
    AD8531
    AD8532
    AD8534
    AD8565
    AD8566
    AD8567
    AD8614
    AD8644
    ADD8504
    ADD8710
    AD8519
    ADSY8401
    AD8529
    AD1870
    AD1871
    AD1877
    AD1974
    ADAU1977
    ADAU1978
    ADAU1979
    ADAU7002
    SSM2602
    SSM26…
  • Sigmastudio unhandled exception pain

    Hi,

    I keep getting unhandled exceptions in  Sigmstudio when I attempt to do link and download. Sometimes, after creating a new project, it will connect, but as I add the bits I want, at some point, it just breaks, and then appears to be stuck with the…

  • FAQ: [#6331] There is error in adau1371 audio testing on bf527-ezkit(2010)

    [#6331] There is error in adau1371 audio testing on bf527-ezkit

    Submitted By: angelia wu

    Open Date

    2010-11-05 05:21:36     Close Date

    2010-11-09 01:09:07

    Priority:

    Medium High     Assignee:

    Cliff Cai

    Status:

    Closed     Fixed In Release:

    N/A

    Found In…