• FAQ: [#6882] Can't use S24_LE format to record audio with adau1361 on bf537-stamp.(2011)

    [#6882] Can't use S24_LE format to record audio with adau1361 on bf537-stamp.

    Submitted By: Vivi Li

    Open Date

    2011-11-15 01:22:05    

    Priority:

    Medium     Assignee:

    Lars-Peter Clausen

    Status:

    Open     Fixed In Release:

    N/A

    Found In Release:

    2011R1     Release:

    Category…

  • FAQ: [#6923] arecord/aplay may crash when test adau1361 audio card in 2011r1 branch(2011)

    [#6923] arecord/aplay may crash when test adau1361 audio card in 2011r1 branch

    Submitted By: Vivi Li

    Open Date

    2011-12-15 22:01:05    

    Priority:

    Medium     Assignee:

    Lars-Peter Clausen

    Status:

    Open     Fixed In Release:

    N/A

    Found In Release:

    2011R1     Release:

    Category…

  • ADAU1361 LAUX and RAUX sampling

    Hi,

    Could you confirm if the LAUX And RAUX inputs can be simultaneously ADC processed as well as played through LHP and RHP ?

    If not, how much would be lag in between the input and output?

  • ADAU1452 serial data clocking for an ADAU1361 simultaneous playback and record

    I am considering a project that would use an ADAU1452 to receive serial audio samples from an ADAU1361, process them, and then send them back to the ADAU1361 for output. The ADAU1361 contains only a single set of BCLK / LRCLK pins, and thus operates fully…

  • Reading max-hold sample values from ADAU1542 to implement automatic ADAU1361 gain configuration

    My project (a fully-custom bass/guitar effects processor) consists of an ADAU1452 DSP, an ADAU1361 codec, and an STM32 microcontroller. Given the vast array of potential input signal levels (active vs passive pickups, direct input from the instrument or…

  • ADAU1361 DC Offset

    Hello,

    we have used the ADAU1361 in a product that will be operational this year and we are quite happy with the way it works. We are pairing it with a Linux box to capture analog audio and doing our captures using the ADI driver adjusted to run ou our…

  • Status of ADAU1361 when the headphone amplifier is not used

    Hello

    I have a question about ADAU1361.

    Question
    Will it be Hi-Z when the headphone amplifier is not used in ADAU1361?

    I would appreciate it if you could reply.

    Best regards,

    Knj

  • ADAU1361 ADC Full-Scale Level with negative PGA gain

    Hello Analog Community,

    The ADAU1361 datasheet states an ADC full-scale level of 1 Volts rms when operated with AVDD = 3.3 Volts. My question is, when using the PGA in single ended mode (line-in) with a gain of -6 dB, will the device accept 2 Volts rms…

  • ADAU1361 differential amplifier not working, no internal bias on input pins - damaged part, or just misconfigured?

    I'm bringing up a new design that utilizes an ADAU1361, and I've run into a bit of a snag that I'm hoping is just due to a misconfiguration of the device, but which I fear is actually evidence that the device itself is damaged (with everything being out…

  • ADAU1361/ADAU1961 About usable frequencies

    Hi,

    I would like to use two products, ADAU1361 / ADAU1961.
    We are judging whether it matches the specifications.
    Below, there are some frequencies that are not in the data sheet, so
    I want you to check if it can be used.

    There are two conditions.
    I think…