• A series of questions about ADATE318

    1. How to get the ibis model of the ADATE318?

    2. What the difference between the pin PPMU_Sx and PMU_Sx? How to use these pins in application?

    3. How to connect the kinds of GND in the application, such AGND, PGND, DGND, DUTGND, VREFGND.

    4. Do you…

  • ADATE318 IBIS model

    Hi ADIer,

     

    Where can I find the IBIS model of ADATE318? I can not do simulation without it.

    I can't find a suitable place to put this request, ADATE318 integrated DACs, maybe I can put it here.

     

    Thanks in advance.

     

    Jason

  • Supply voltage for temp sensor ADATE318

    What is supply voltage (VDD_TERM) for temp sensor ADATE318. I did not find this information in the datasheet.

  • RE: questions about ADATE318

    The 1.2k is the typical value for the Ron for the Ext Sense Switch (as seen on Fig 136 of page 78 of the datasheet). If you check the specs, this switch resistance can go up to 2.5kOhms.

  • RE: Question about PCB design for efficient heat control of ADATE318

    Hi Se-woong,

       My Apologies on the very late reply,  I have run through our archives and I couldn't find any PCB design or layout guide regarding the ADATE318, I would still point to the Power Supply, Grounding, and Decoupling Strategy Section of the ADATE318…

  • Maximum Recommended PMU Load Capacitance

    What is the maximum recommended PMU load capacitance for the ADATE304?

     

    The maximum recommended PMU load capacitance is 2000pf.  
    The ADATE304 and ADATE318 are both characterized with a load capacitance of
    200pf and 2000pf.
  • Inquiry on DUT pin voltage rating of ADATE318.

    Dear,

    Would you please check the below inquiry for ADATE318?

    - DUT0 pin voltage rating

    Relay On for HVOUT and then the DRV_LOW_LEAK line is switched off for DUT0.

    In case of 14V HVOUT level, it needs to check if there is no problem on DUT0 port(any…

  • ADATE318: What supply voltage do I use for VDD_THERM?

    What is the supply voltage for pin 1 (VDD_TERM) to supply temperature sensor?
    There is no information in the datasheet. 

     

    The VDD_Therm pin is to be tied to the VDD power supply.  The naming was
    intended to label it as an VDD pin that…
  • TAGS LIST: Amplifiers

    AD600
    AD602
    AD603
    AD604
    AD605
    AD8264
    AD8330
    AD8331
    AD8332
    AD8334
    AD8335
    AD8336
    AD8337
    AD8338
    ADL5246
    ADL5330
    ADL5331
    LTC6412
    HMC6187G
    HMC997G
    HMC996
    HMC694G
    AD8368
    AD8351
    AD8367
    AD75071
    AD552…