• ADATE209 Propagation Delay

    Hello Community,

    I want to use multiple ADATE209 to create synchronized outputs. I think the specs fit quite well to my application. Then I stumbled over the huge tolerance in propagation delay starting from 300ps up to 1400ps. Can someone tell me, which…

  • Question of ADATE209

    Hi Sir,

    1.According to ADATE209 datasheet Figure 13 CLC Disable and Enable, Showed CLC Enabled sign-wave amplitude small than Disabled, which result different than others.Is that correctly?

    2. I can’t understand the Figure 14 chart, Are DROUT1 and DROUT2…

  • Need support of ADATE320 and ADATE209

    Hi 

        I am writing for support of ADATE320 and ADATE209.

    In our project, ADATE320 is uesd to realize 1.6 Gbps LVDS signal adjust.

    Original LVDS signals comes from FPGA (Xilinx HP bank). There is my first

    question, could you give us a circuit of typical…

  • ADATE209 S parameter

     Hi Sir,

    Does ADI can provide ADATE209_Simulation Model(S-parameter)?

    My customer need to above for a simulation ,tks!

     

  • More design guide about ADATE320 and ADATE209

    I could get only the datasheet in the website. Is there more design guide, like tools for the register configuration,whitepaper about the mode in application, or the DMO board?

    Thanks!

  • ADATE209 simulation model (IBIS) availability ?

    After a long time of no response to my previous question on the ADATE209,

    I edited the contents of this post.

    Does AnalogDevice support simulation model for ADATE209 device ?

    From the product page, I cannot find any.

    From the local sales, I heard…

  • RE: Recommended replacement of AD53513

    Hi jiawf,

         Thank you for taking interest in our ATE products. The AD53513 is a Quad Ultrahigh-Speed Pin Driver with High-Z and VTERM Modes. Given that, the closest which is now still in production is the ADATE209. To better help, can I have additional…

  • TAGS LIST: Amplifiers

    AD600
    AD602
    AD603
    AD604
    AD605
    AD8264
    AD8330
    AD8331
    AD8332
    AD8334
    AD8335
    AD8336
    AD8337
    AD8338
    ADL5246
    ADL5330
    ADL5331
    LTC6412
    HMC6187G
    HMC997G
    HMC996
    HMC694G
    AD8368
    AD8351
    AD8367
    AD75071
    AD552…