FAQ
Is there an IBIS model available for the ADAS3022?
Yes, please follow the link below:
http://www.analog.com/en/analog-to-digital-converters/ad-converters/adas3022/pro
ducts/tools-software-simulation-models/index.html
How to configure IN1 channel alone and get SPI (SDO)output in ADAS3022?
Hi,
We are using EVAL-ADAS3022EDZ board to evaluate ADAS3022 chip.
We intended to measure +/- 5V using this board & configuration value we have is 'F57E'.
Below is the result.
VREF IN results +2.844 Voltage.
We are expecting linear output…
Hi,
I'm working with the ADAS3022 and would like to convert the 16 bit codes it produces into voltages. I am currently using the following formula:
V = (CODE / GAIN) * (2*VREF)/32768
This produces reasonable values, but it appears that the LSB value…
Hi,
ADAS3022 Evalution board using External Spi communication we are modified jumper . We are facing issues for differential voltage measurements.Spi communication we got only one channel output and remaining output not correct. Please help me.
Hi,
I am using ADAS3022 (ADC Board) interfacing with HDK as shown in the below figure
With the clock frequency of 1MHZ.
Below table shows the expected output for the given input voltage
Below is the output table which I got
Input Voltage |
ADC… |
RIO,
There is no requirement for using a Low Drop Out Regulator as long as you understand the potential sources of error that can be introduced through the supplies. Please note that the switching frequency for the regulator you are proposing falls within…