• ADAS1000-4BCPZ And ADAS1000-2BCPZ

    Hi,

      Presently  im working on medical equipment for ECG data using ADAS1000-4BCPZ and ADAS1000-2BCPZ.For 6Lead and 12 Lead .Kindly help me out in providing Sample code for reading the ECG data,Lead On ,Lead Off status...

    Thanks in advance

  • RE: ADAS1000-4 and ADAS1000-2 configuration for 12 leads

    Dear Catherine, 

    Can we test this configuration on the ADAS1000 EVM. If yes, Please let me know the settings to be done.

    Thanks 

  • ECG 12D ADAS : could i use 2 ADAS1000 (1 master 1 slave) instead of an ADAS1000-2

    Hi everyone,

    Because of the current component shortage, we are wondering if we can replace our ADAS1000-2 by a second ADAS1000 in order to get ECG 12D ? We tried to replace it by an ADAS1000 on an existing board but i can't get a frame from the slave…

  • ADAS1000 Family

    Hi everyone

    I have a project that its intent it's to acquire a 6 leads ECG, but because of the application, we are only able to use 3 electrodes that would be (LA, RA, LL). My question is the following:

    Is there a configuration where we can loop the…

  • SPI communication between the ADAS1000-3 and the Intel Edison platform

    Hello.

    I am currently working on the development of an ECG, and I have been using several alternatives. I mainly work with the AD8232, but I have started working with the ADAS1000-3 for a theme of having greater features and functions.

    I am using the…

  • Choice of ad8232 or ADAS1000-3 chip to take ECG signals

    I am currently developing a device that analyzes the ECG signals to basically study the bit rate. I am using the AD8232, but I have been evaluating the possibility of changing to the ADAS1000-3, but looking in its datasheet I found a part that indicates…

  • RE: AD8232 vs ADAS1000-3

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • what does the "-3" on the brand of ADV7390/1/2/3 and ADV7340/1/2/3 indicate?


    The latest revision of the encoder has the -3 version branded on it's package. The revision code of the encoder can be read back from register 0xBB bits 7:6. 01B indicates the latest revision.

    Further information on the change made to this version…

  • RE: ADAS1000-3 and analog switch

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • ADAS1000 three lead configuration

    Dear engineer :

            Regarding the configuration of the three-lead ECG, if we want to select the I lead as the main lead, that is, the LL as the reference drive lead, the register configuration is as follows:

    0x05 0x85a0202b, 0x03 0x830139ff,  I would like…