• ADAS1000 ACLO Operation

    Purpose: The ACLO block within the ADAS1000 is used to help user identify if an electrode has fallen off or if the connection is poor (higher impedance). This document captures some detail around the operation of the block and using it.

    Implementatio…

  • ADAS1000: DC lead off detection.

    Hi

    I am testing DC lead off detection in ADAS1000 configured in common electrode mode, I have routed RA to CE  on the board. I have tested the lead off detection when

    1. 1.3V is contributing to RLD 

    2. When RA, LL and LA are contributing to RLD.

    - In both…

  • ADAS1000. RLD simulation with external components.

    I have simulated the RLD with the external components in the ADAS1000 with the SW1-SW5 opened and RFB = 4M RIN =40k. I am not sure if the simulation is correct due to the negative values.
    RLD_externalcircuit.rar

  • ADAS1000: Shift in amplitude of ECG

    Hi,

    I am trying to configure ADAS1000 in the electrode mode as shown in the figure below.

     

    When I record the data in Single ended mode, with gain 4.2, The amplitude of ECG is shifting to 2.0mv(originally fed ecg amplitude 1.0mv). Please let me know why…

  • ADAS1000 questions

    My questions to ADAS1000-4:
    a)  Does ADAS1000-4 also work with only two electrodes e.g. LA and RL ?
    b)  How does the respiration measurement (respiration-path) work and where do
    you have to connect the three outputs/inputs ?
    c)  Does each ECG input…

  • The ADAS1000 device was designed as an ECG front end. Can I use it for EEG applications?

    Q: The ADAS1000 device was designed as an ECG front end. Can I use it for EEG applications?

    A: Firstly let's look at the differences between an ECG and an EEG signal:

    ECG:

    An ECG (electrocardiogram) is 'sensed' on the surface of the patient, on the…

  • ADAS1000 DRDYb operation

    The purpose of this document is to describe a little more about the DRDYb operation of the ADAS1000. This should be read in conjunction with the ADAS1000 datasheet descriptions.

    There are two modes of interfacing operation within the ADAS1000,

    • read/write…
  • ADAS1000 Input Range

    Hi all,


    I'm usisng a SoC ADAS1000 on a school projetc and I would like to know what's the minimum input range that the front-end can read? The datasheet says it's 300mV, but in the projects available online,made by others, no one is using an external…