• ECG 12D ADAS : could i use 2 ADAS1000 (1 master 1 slave) instead of an ADAS1000-2

    Hi everyone,

    Because of the current component shortage, we are wondering if we can replace our ADAS1000-2 by a second ADAS1000 in order to get ECG 12D ? We tried to replace it by an ADAS1000 on an existing board but i can't get a frame from the slave…

  • Gang Mode ADAS1000 and ADAS1000-2 - OPSTAT Register always busy

    Hello all,


    I'm in the process of writing a software driver for an ADAS1000 and ADAS1000-2 ECG front end and I'm getting problems in the gang mode. I tested read frames in the master (ADAS1000) and all worked well but when i tried connect both the Configuration…

  • RE: ADAS1000-4 and ADAS1000-2 configuration for 12 leads

    Dear Catherine, 

    Can we test this configuration on the ADAS1000 EVM. If yes, Please let me know the settings to be done.

    Thanks 

  • Wireless ECG sensor using ADAS1000 and ADAS1000-2

    I want to design a wearable ECG sensor that can transmit the sensory data via BT/WiFi. I am thinking of using ADAS1000 and ADAS1000-2 for ECG measurements and a separate BT module that has SPI interface for wireless transmission. Does anyone have any…

  • ADAS1000-4BCPZ And ADAS1000-2BCPZ

    Hi,

      Presently  im working on medical equipment for ECG data using ADAS1000-4BCPZ and ADAS1000-2BCPZ.For 6Lead and 12 Lead .Kindly help me out in providing Sample code for reading the ECG data,Lead On ,Lead Off status...

    Thanks in advance

  • RE: ADAS1000 : DC-lead off detection not working for RA, LA and LL

    Hi,

    Can you try the suggestions mentioned in DC Lead-Off and High Gains section of the ADAS1000/ADAS1000-1/ADAS1000-2 (Rev. C) (analog.com) datasheet. RA, LA, and LL are also connected to common mode amplifier so that might also be causing this issue.

  • About using the software SPI to connect the ADAS1000 and ADAS1000-2

    hello

    I think when you use the ADAS1000, you are using the hardware SPI. Now my project is using ADAS1000 and ADAS1000-2, and I need to use the analog spi interface. How do you use it? I hope to give me some Thank you, thank you

  • Register configuration for ADAS1000-4 and ADAS1000-2 12 Leads configuration

    I am working with these 2 ICs, and I have already configured registers for get working in 12 leads configuration measurement. You can see this in the previous post. However the signal recollected in the second chip is not the expected.

    As you can see…

  • RE: ADAS1000: Why the amplitude of ECG is changing when I am trying to use electrode configuration?

    Hi,
    Please note that user gain calibration is required for gain=4.2.. Please see gain calibration section in the datasheet 
    ADAS1000/ADAS1000-1/ADAS1000-2 (Rev. C) (analog.com)

    Regards,
    Mark

  • ADAS1000 three lead configuration

    Dear engineer :

            Regarding the configuration of the three-lead ECG, if we want to select the I lead as the main lead, that is, the LL as the reference drive lead, the register configuration is as follows:

    0x05 0x85a0202b, 0x03 0x830139ff,  I would like…