• ADAR1000 Purchase

    Hi,

    can anyone provide me with contact information for how to get a quote for the ADAR1000 chip (not the eval board)?  I have been unable to get a hold of anyone at ADI that knows anything about this chip and all the contact information posted online seems…

  • ADAR1000 SPI

     Hello, I am using ADAR1000 but unfortunately, there is no reference source code. I could not find anywhere. Just we have SPI PROGRAMMING EXAMPLE in the Datasheet. I want to make and control the SPI communication protocol without using GUI. Can you provide…

  • ADAR1000 questions

    Hi,

    All document references below refer to the ADAR1000 datasheet (Rev. A) and to

    I) Questions related to beam stepping
    ---------------…
  • ADAR1000-EVALZ

    Hi all,

    ADAR1000-EVALZ is include the SDP-S ?

    "The ADAR1000-EVALZ can be driven by a Windows-based computer through USB using ADI's Standard Develop Platform Serial adapter (SDP-S). External serial programming and other digital control signals can also…

  • ADAR1000-EVALZ

    Hi all,

    ADAR1000-EVALZ is include the SDP-S ?

    "The ADAR1000-EVALZ can be driven by a Windows-based computer through USB using ADI's Standard Develop Platform Serial adapter (SDP-S). External serial programming and other digital control signals can also…

  • ADAR1000 Measurements

    WIth the ADAR1000 and connectors for every port (4 TX and 4 RX and 1 RFIO) do 7 ports need to be terminated in a 50 ohm load for a 2 port measurement? Or only RX ports terminated with 50 ohm if only the RX channels enabled?

    Also, with my own evaluation…

  • ADAR1000 Labview

    Does anyone have a LabVIEW GUI for the ADAR1000 they would be willing to share? First time trying to program a chip via SPI and have not gotten anything to work. Any help would be greatly appreciated. Thanks.

  • ADAR1000 50ohm termination

    Hi. I want to use adar1000 to implement phased array antenna.

    When using only the Tx port of the chip, should I connect a 50 ohm resistor to the Rx ports to make a 50 ohm termination?

    Or is it possible to open the chip pad because it is internally terminated…

  • ADAR1000 Gain Setting

    I am having a problem with a phased array board equipped with ADAR1000 and ADTR1107, which will not stop oscillating unless the front-end gain is reduced by at least 15dB from the maximum. The reason for the oscillation is that the layout design of the…

  • ADAR1000 in LTspice

    Is LTspice macro model for ADAR1000 available ?