• ADAQ7768-1 Voltage Conversion

    I am programming a library for the ADAQ7768-1 (together with the Mikroe DAQ click board) for use with an Arduino using SPI communication. I'm able to read the several provided registers. But I'm wondering about converting the raw data to the actual voltage…

  • ADAQ7768-1 CRC

    Hello,

    I have enabled CRC Check (EN_SPI_CRC=1,CRC_TYPE=0)

    Then I use single-read mode from ADC_DATA. I received CRC but I think it is different than it should be.

    Eg.

    I receive data: 0xff 0xfb 0x47 (adc_buf[1],adc_buf[2], adc_buf[3])

    According to datasheet…

  • RE: Request a reference schematic about connecting betweeb Slave boards with ADI BMS ICs (LTC6802-1/LTC6811-1/LTC6812-1/LTC6813-1)

    Hi Se-woong,

    We currently do not have multi-module configuration evaluation schematic/model. You can follow the application circuit provided in the datasheet of LTC6811-1 (page 79-80). Thank you!

    Regards,

    Audi

  • LTC9101 DC3159A-A 1/5W and 1/10W resistance

    Hi,

    In the LTC9101-1 EVK DC3159A-A circuits, the data isolator is T1 7490100143.

    The peripheral resistors are 49.9, 10Meg, and 100K ohm. Just wondering the reason you use high power tolerance such as 1/5W and 1/10W resistor ?

    Can we use normal resistors…

  • LTC3114IDHC-1#PBF & LTC3114IDHC-1#WPBF

    Dear Support,

    Good day,

    Please help me on the difference between part numbers below?

    What is the "W" meaning in the part number TC3114IDHC-1#WPBF?

     

    LTC3114IDHC-1#PBF

    LTC3114IDHC-1#WPBF

  • RE: Questions for LTC6811-1, LTC6812-1

    Dear Abhishek,

    Thank you for your kind answer.

    But additionaly my customer asks that they want to know the maximum power specification of Zennor diodes in LTC6812-1 and LTC6811-1.

    (Its zennor diodes are located inside of LTC6812-1 and LTC6811-1 and Cx…

  • Difference between LTC3114IDHC-1#PBF & LTC3114IDHC-1#WPBF

    Dear Support,

    Good day,

    Please help me on the difference between part numbers below?

    What is the "W" meaning in the part number TC3114IDHC-1#WPBF?

     

    LTC3114IDHC-1#PBF

    LTC3114IDHC-1#WPBF

     

  • LTM4650AIY-1#PBF vs LTM4650AIY-1#3NSPBF

    Could anyone explain what 3NS means on part numbers such as LTM4650AIY-1#PBF vs LTM4650AIY-1#3NSPBF ?

    I cannot find any information.

    thank you

  • "AD5940_WriteReg(REG_AFE_SWMUX, 1<< 1) " is Valid?

    HI.

    I have a question about some code in BATImpedance.cpp.

    ------------------------

    AD5940_WriteReg(REG_AFE_SWMUX, 0);

    or 

    AD5940_WriteReg(REG_AFE_SWMUX, 1<< 1);

    -----------------------

    In the datasheet REG_AFE_SWMUX  (0x0000235C)

    [2:0] reserved , 

  • RE: LTC6363-1 replacement LTC6363-1 replacement LTC6363-1 replacement

    Hi Mamzi,

    Have you checked on our authorized distributors? What package do you need?

    You can check Analog Devices' parametric search for single-ended to fully differential amplifiers

    Single-Ended to Differential Amplifiers Fixed Gain Selection

    Regards…