2009-03-09 16:16:14 Mounting jffs2 partition
Steven Vacca (UNITED STATES)
Message: 70622
I am having troble getting my jffs2 partition mounted.
My Environment: bf537 dev unit, m25p128 FLASH
--------------------------------------
Kernel boot-up…
HMC637ALP5E on a 16 x 16 Prototype Plate with X-MWprobes
2011-03-16 01:16:36 SD card with BF53x
Sergio Morales (COLOMBIA)
Message: 98955
HI,
I'm trying to use the SD card driver over SPI, this is the connection used: wiki.linuxencaja.net/images/6/63/Sch_uSD.jpeg
I have kernel version 2010R1. Reading…
2008-02-01 16:16:34 API for GPIO Wakeups
Christopher Harrsen (UNITED STATES)
Message: 50582
I would like to use the API for GPIO wakeups. This is a kernel space API. Does this mean I have to compile my application to run in Kernel space. How do…
2010-04-16 14:16:51 New to uClinux and Blackfin
Matthew Sacrey (UNITED STATES)
Message: 88529
Hi
I'm working a class project involving a BlackFin 548 evaluation kit. My tea inherited the project from a previous year's group, who installed uClinux…
2008-02-11 16:16:27 Getting Started with Skyeye & bf533
Michal Steyn (AUSTRIA)
Message: 50910 I am new to Skyeye and uCLinux. I am working on a project using a Blackfin bf533 processor.
I am trying to configure my system but I cannot get any…
2010-06-16 16:14:47 2009R1.4 netflash w/ HMAC_MD5 doesn't build
Andrew Kohlsmith (CANADA)
Message: 90344
It can't find openssl/sha.h. The file exists both on the host (/usr/include/openssl/sha.h) as well as in the uClinux-dist (lib/libssl/openssl…
2008-12-16 22:13:16 How to optimize compiling ucLinux time?
Tony Liu (CHINA)
Message: 66775
Dear all,
I'm working on colinux & build uclinux for my board. How to optimize compiling uclinux for saving time?
For u-boot can using RAMDisk…
2010-03-16 07:16:34 Kernel panics : Cramfs as root file system
Santhosh Kumar (INDIA)
Message: 87251
Am trying to use cramfs in flash memory as my root file system. When booted my bf527 device with vmImage, kernel panics with error message "Kernel…
2011-01-16 16:20:02 Problem loading sound drivers in /etc/rc
Jay Ku (UNITED STATES)
Message: 97479
I have a SSM2603 codec working on my custom BF537 board (running 2010R1 distro). I've built all the drivers as modules, and if I load them manually…