• ADA4960-1 : Is there PSRR data available?

    Is there PSRR data for ADA4960-1, none is provided in the datasheet
    specifications?

     

    We do not normally specify PSRR for high speed amplifiers. There is no AC data
    available but we do have DC data from the tester. According to the test…
  • ADA4960 Input Range, Output swing limit, Simulation in ADI Diff-Amp Calc

    Hello,

    I am preparing to use the ADA4960 in a new design and need some clarification on the input voltage range, and the output swing limit.  I am afraid the datasheet is not totally clear, and attempting to model the part in ADI Diff-Amp Calc has further…

  • ADA4960 Input Range, Output swing limit, Simulation in ADI Diff-Amp Calc

    Hello,

    I am preparing to use the ADA4960 in a new design and need some clarification on the input voltage range, and the output swing limit.  I am afraid the datasheet is not totally clear, and attempting to model the part in ADI Diff-Amp Calc has further…

  • ADA4960-1 output problem

    Hi engineers:

    The J11 input is pulse signal .VPP is 600mV(differential),rise time :2ns, fall time:1.6ns.Then I test the R16 and R17 differential signal.

    How can the waveform as shown in the diagram be eliminated? Thank you!

  • ADA4960-1 Diff In to SE Out

    Would like to use AD9959 DDS in Super Nyquist application for frequencies from 1.4-1.5GHz. No suitable transformers exist in this band with CT, so considering using ADA4960-1 as interface to the DAC outputs. Curious if this would be a good device to use…

  • RE: ADA4960-1 work for differential input to single-ended output?

    Hi Erin,

    Sorry for the late reply. For your first question, Yes you may use ada4960-1 as single-ended-output, but keep in mind that if you'll use ada4960-1 as single-ended-output you will sacrifice the gain. The resulting gain will be the half of the…

  • RE: Questions for LTC6811-1, LTC6812-1

    Hello,

    Would you share your answer about "for maximum power capacity of zener diode - we will look into this and get back to you soon."?

    My customer still need your answers.

    Regards,

    Se-woong

    PS.

    Jay shin is moved to other company.

    So I…

  • LTM4650AIY-1#PBF vs LTM4650AIY-1#3NSPBF

    Could anyone explain what 3NS means on part numbers such as LTM4650AIY-1#PBF vs LTM4650AIY-1#3NSPBF ?

    I cannot find any information.

    thank you

  • "AD5940_WriteReg(REG_AFE_SWMUX, 1<< 1) " is Valid?

    HI.

    I have a question about some code in BATImpedance.cpp.

    ------------------------

    AD5940_WriteReg(REG_AFE_SWMUX, 0);

    or 

    AD5940_WriteReg(REG_AFE_SWMUX, 1<< 1);

    -----------------------

    In the datasheet REG_AFE_SWMUX  (0x0000235C)

    [2:0] reserved ,