Hi,
I would like to use ADA4950-2 as a buffer to measure noise with my chip. May I have the original output noise data for ADA4950-2 as shown in Figure38 in the datasheet? Thanks!
Best,
Nancy
Hi,
I would like to use ADA4950-2 as a buffer to measure noise with my chip. May I have the original output noise data for ADA4950-2 as shown in Figure38 in the datasheet? Thanks!
Best,
Nancy
Hi,
Does ADA4950-1/2 power down pin have an internal PU or PD resistor ?
Datasheet does not mention this.
Have a nice day...
Hi,
I am using ADA4950-2 Differential Amplifier to make differential my DC signal. I hve a output common mode voltage of 1.5 V for this chip
I have two questions:
1) When nothing is connected to INA- and 1.65 V is connected to INA+ I see 1.47 V(apporixmately…
Hi,
Attached is the board file for ADA4950-2. The old evaluation board for ADA4950-2 is obsolete and is replaced by EVAL-FDA-2CPZ-24.
Regards,
Goz
Hi all,
I'm using ADA4950-1YCPZ amplifiers as the last stage in a preamp before driving an AD9650. The ADA4950 is powered by +/-5V supplies. The unity gain inputs (pins 2 and 3) are driven by ADA4897s powered by the same +/-5V supplies. Pins 1 and…
Hi,
i want to use ada4950-1 as an single to differential amplifier with the gain of 1 and output common voltage at 500mv , i used adr130 to produce the 500mv and connected directly its output to the vocm of ada4950.when i power up the board and just measure…
Hi,
We do have a catheter cable length of 2.4 meter , trying to understand if the amplifier ADA4950-1 will be able to drive the same or not?
We have set this for a gain of 2. The input level from the FPGA is driven as 2.4V p-p, output of the ADA4950-1 is…
Can you provide advice for proper design considerations for the following questions:
1) The signal we're passing is only operating between 20Hz and 15Mhz. Would reducing the Bandwidth of the device help prevent oscillations, and if so what would…
Hi,
I am goning to distribute a common 40 MHz clock to 2 DDSs and 2 ADCs. Will AD9577 work for this purpose? If not, do you have any suggestion?
The ADC needs 5 V CLK and the DDS needs 1.8 V CLK.