Hi,
I would like to use ADA4950-2 as a buffer to measure noise with my chip. May I have the original output noise data for ADA4950-2 as shown in Figure38 in the datasheet? Thanks!
Best,
Nancy
Hi,
I would like to use ADA4950-2 as a buffer to measure noise with my chip. May I have the original output noise data for ADA4950-2 as shown in Figure38 in the datasheet? Thanks!
Best,
Nancy
hi, i am complicated with ada4950 evaluation board pcb .is there any gerber file for that?
Hi everyone,
Because of the current component shortage, we are wondering if we can replace our ADAS1000-2 by a second ADAS1000 in order to get ECG 12D ? We tried to replace it by an ADAS1000 on an existing board but i can't get a frame from the slave…
On the evaluation board for the LTC3114 Diode D2 connects to SW2 on the IC, What does it do, and under what conditions is it needed? We are supplying 12V at 1amp from 9 to 30V input to external customer supplied devices, these may have there own input…
Is it possible the device is somehow getting into HMC mode SPI rather than open mode when you have the ref div = 1. I cannot think of a reason why this would be the case, but the HMC SPI interface has been known to have issues at times with selecting between…
Dear Sir/Madam,
I am after some PCB routing advice on connecting one ADA4857-1(gain of 2) to four ADA4857-1 (gain of 1).
The delay between the ADA4857-1 is not important just signal quality.
Regards Joe
In our application we are using link ports to transfer data between an FPGA and the DSP at periodic intervals. We setup link port 1 (LP1) in DMA receive mode as prescribed in the HRM (pages 15-15, 15-16). After the data is received, LP1 and it's DMA are…