• ADA4950-1: temp drift

    Please let me know the temperature-drift SPEC for the gain of ADA4950-1.

    They find that the related curves are shown in Figure 9 and Figure 10 in the
    datasheet. Now they want to get the specific values of the temperature drift.

     

    Don…
  • ADA4950-1/ capacitance load query

    Hi,

    We do have a catheter cable length of 2.4 meter , trying to understand if the amplifier ADA4950-1 will be able to drive the same or not?

    We have set this for a gain of 2. The input level from the FPGA is driven as 2.4V p-p, output of the ADA4950-1 is…

  • ada4950-1 vocm problem?

    Hi,

    i want to use ada4950-1 as an single to differential amplifier with the gain of 1 and output common voltage  at  500mv , i used adr130 to produce the 500mv and connected directly its output to the vocm of ada4950.when i power up the board and just  measure…

  • ADA4950-2 POWER-DOWN (PD)

    Hi,

    Does ADA4950-1/2 power down pin have an internal PU or PD resistor ?

    Datasheet does not mention this.

    Have a nice day...

  • RE: LTC6363-1 replacement LTC6363-1 replacement LTC6363-1 replacement

    Hi Mamzi,

    Have you checked on our authorized distributors? What package do you need?

    You can check Analog Devices' parametric search for single-ended to fully differential amplifiers

    Single-Ended to Differential Amplifiers Fixed Gain Selection

    Regards…

  • RE: Sporadic ADA4950 failures

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • ADA4950-2 Input Current Specification

    Hi,

    I am using ADA4950-2 Differential Amplifier to make  differential my DC signal. I hve a output common mode voltage of 1.5 V for this chip
    I have two questions:

    1) When nothing is connected to INA- and 1.65 V is connected to INA+ I see 1.47 V(apporixmately…

  • LTC3114-1 evaluation board SCP-LTC3114-1-EVALZ

    On the evaluation board for the LTC3114 Diode D2 connects to SW2 on the IC, What does it do, and under what conditions is it needed? We are supplying  12V at 1amp from 9 to 30V input to external customer supplied devices, these may have there own input…

  • ADA4950-2 Output Noise Data

    Hi,

    I would like to use ADA4950-2 as a buffer to measure noise with my chip. May I have the original output noise data for ADA4950-2 as shown in Figure38 in the datasheet? Thanks!

    Best,

    Nancy