• RE: ADA4938-2 problem

    Hi Denkins,

    Thank you for your interest in ADA4938 and AD9253. I'm sorry but I cannot see the schematic clearly. Would you please confirm what the ADA4938 supply voltages are?

    I believe Jino's point is that, depending on the amplifier supply voltages…

  • exact value of the differential output impedance of the ADA4938-1 or ADA4938-2

    What is the exact value of the differential output impedance of the ADA4938-1
    or ADA4938-2. Is it 2ohm or 5ohm or 20ohm?There are S parameter plots S11 nad
    S22 in the datasheet but I don't know to which circuit they apply to or to
  • ADIsimPE How to use diffrential amp?

    Hi, all.

    I'd like to simulate diffrential amp(ADA4938-2) by using ADIsimPE.

    So I imported ADA4938-2's spice model and define the symbol,

    ADIsimPE doesn't show the correct symbol.

    How do I define the correct symbol?

  • RE: AD9613 input driver question

    By the way ... I've paid an attention to the caption of figure 47 ... " Figure 47. Differential Input Configuration Using the ADA4938-2 " While the OpAmp shown is ADA4930-2.

  • Difference between ADA4938-1ACPZ-R2 and ADA4938-1ACPZ-R7

    Is there any difference between the part numbers  ADA4938-1ACPZ-R7 and ADA4938-1ACPZ-R2 other than the sample ordering quantity?

  • RE: ADA4938 Output Termination for Driving SMA Cable

    Hi Stephen,

    The actual output impedance of the ADA4938 is not directly stated in its datasheet. However, also like an op amp, the ADA4938 has a low output impedance.

    For the proper termination of the output of the ADA4938 to drive a signal through…

  • ADC driver for AD9255

    I'm planning to use the AD9255 single 14 bit ADC with DC coupled input signals in the dc - 20 MHz range.

    Because of the DC coupled requirement I am looking at ADC driver amplifiers instead of a transformer.

    The AD9255 web page recommends the ADA4937…

  • RE: AD9268采集脉冲波形的疑问

    AD8138可以作为 ADC driver,但是其-3dB带宽只有320MHz,所以最好采用ADA4938-2

  • RE: AD9265 cmos clock driver

    My signal is IF signal at 10.7MHz, which can go -50dBm to 0 dBm.

    I am thinking to use AD9650 instead of AD9265.

    to convert single ended to differential i am planning to use ADA4938.

    I will add 10dB gain by using ADA4938.

    How much max gain ADA4938…