• RE: Correct layout of ADA4937-2

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: How to get proper footpring for ADA4937-2

    Hi Eric,

    ADA4937-2 comes with a package option of CP-24-10 which is compliant to JEDEC Standars MO-220-WGGD-8. We apologize that there is no bxl file available in the product page. We will have it updated.

    Regards,
    Jino

  • Diff-Amp Calculator has a problem with ADA4937?

    Trying to run simulation on ADA4937 with Diff-Amp Calculator, and no matter what the input or gain is, it thinks the input is clipped. What's going on?

  • How to drive AD9637 use 3 pcs ADA4937-2?

    How to drive AD9637 use 3 pcs ADA4937-2? What's the connnection about the 6 Vocm pins of 3 pcs ADA4937-2 to the Vcm pin of AD9637? Thanks!

  • ADA4937-2作为AD9637驱动问题

    你好,请问釆用三片ADA4937-2作一片AD9637的前置驱动,AD9637的VCM和6路ADA4937的V0CM怎么连接?谢谢!

  • Inquiry about the design of the AD9258 and the ADA4937-1

    Hello,

    My customer will use ADA4937-1 and AD9258 at repeater application.

    1. Input voltage range of the Vocm pin in the ADA4937-1 is min 1.2V to max 3.8V. However, the VCM output of the AD9258 is 0.9V.

        The voltage ranges between the Vocm pin and the…

  • Pluto - 2 Rx and 2 Tx using MATLAB

    Hi,

    I would like to setup the SDR Pluto to operate in 2 Tx and 2 Rx mode.

    I have followed the steps in the following video : https://www.youtube.com/watch?v=ph0Kv4SgSuI

    However, I am unsure how to setup and control the 2nd transmitter or receiver. 

  • RE: ADA4940-2, issue on creating 2 differential signals around 0V

    Hi, 

    With a bit late, thanks for this suggestion.

    By applying -0.2V to R3, this circuits can convert 0 to 0.4V to a balanced -0.2 to 0.2V .

    It has been checked on the eval board.

  • ADV7611 YCbCr 4:2:2 SDR issue

    I am trying to configure ADV7611 to output 1280x1024 video in 16-bit SDR ITU-R BT.656 4:2:2 Mode 0.

    In free-run mode with blue background I get "0xFF00, 0x0000, 0xFF00, 0x0000..." pixel data, but it is 1280 LLC-period wide DE window between HSyncs…

  • A question regarding LTM4671 parallel 2+2 mode.

    Hi ADI support team. I use LTM4671 in my new design. The datasheet of this device is here: www.analog.com/.../LTM4671.pdf I wonder whether there are two mistakes in the figure2 of datasheet? For 2+2 parallel application, I think PHMODE0 must connect to…