Hi
What is the FIT rate for ADA4932-2
Regards
Sai Kiran S
We have been using ADA4932-2 in our designs. it was working fine for us.
Now they are not available for purchase.
My requirement is 160MHz BW, differential input to differential output amplifiers.
the voltage will is positive and negative 3.3V.
Could…
Hello,
The ADA4932-1 availability at distributors is very low. Only Arrow seems to have any in stock (and only a quantity of 10). Are there projections for when this part will again be widely available? Could you also please suggest the closest alternative…
Hello,
I want to use ADA4932-2 as ADC driver for the ADC AD7768, but my frequency of interest is DC to 100 KHz and input power level in the range of -90 dBm to -10 dBm.
In the datasheet the dynamic performance for frequency less than 100 KHz is not mentioned…
Hi all,
I have downloaded the ADA4932 model from the web. I am using the circuit as shown in the attachment.
I think it is available without being clamped, but when I run the simulation in LTspice, it is clamped as shown in the attachment.
I think this…
Hello,
The ADA4932-1 datasheet states "Can be used with gains less than 1". How much less than 1 while remaining stable? Would a gain of 1/3 be ok for stability? I'm planning 1500 = RF, 500 = RG. Datasheet Figure shows very modest peaking for Gain =…
请教一下ADA4932-2的问题,单端转差分和差分转单端的电路接法,实际调试过程中,按照附件的连接方法,差分转单端使用±5V供电,但是上电之后,电源之间会相互影响,+5V会拉低到0V;还有单端转差分的电路中+OUT1、-OUT1、和+OUT2、-OUT2输出的共模电压不一致,不知道什么原因?