• AD9235, ADA4932-1 spice models

    Hello! Could I get AD9235, ADA4932-1 spice models?

  • ADA4932-1 availability

    Hello, 

    The ADA4932-1 availability at distributors is very low. Only Arrow seems to have any in stock (and only a quantity of 10). Are there projections for when this part will again be widely available? Could you also please suggest the closest alternative…

  • ADA4932-1 minimum gain

    Hello,

    The ADA4932-1 datasheet states "Can be used with gains less than 1". How much less than 1 while remaining stable? Would a gain of 1/3 be ok for stability? I'm planning 1500 = RF, 500 = RG. Datasheet Figure shows very modest peaking for Gain =…

  • ltc2159i+ada4932-1

    i want to use ada4932-1(single to diff) to drive ltc2159, the ada4932-1 input signal is 2vpp,and the max freq is 2mhz,and i want to use ac couple between ada 4932-1 diff out and ltc2159 input.how can i design schematic?or  other drivers  fit for ltc2159…

  • ltc2159i+ada4932-1

    您好:我想让ada4932-1单端转差分交流耦合方式驱动ltc2159i,我中频输入信号最高频率为2mhz,信号幅度为1vpp,拟采样率设为10mhz,请问差放与adc之间的驱动电路怎么设计?另外是否还有别的更合适的差放匹配adc?

  • The common-mode voltage pin about AD9643 and ADA4932-1

    Hi,all

    I plan to use two ADA4932-1 to drive one AD9643 in my design.Now I have some questions and need your help.

    1.Whether the Vocm pin  is a input pin or a output pin?In my opinion ,its a output pin,but its described as a input pin in the datasheet…

  • RE: Error in LTspice with ADA4932

    Hi 

    May I ask if this is where you were able to get the ADA4932 spice model
    ADA4932-1 Datasheet and Product Info | Analog Devices?

  • Use full differential amplifier with gain less than 1 AD8139 or ADA4932-1

    I'm planning to use AD8139 or ADA4932-1 to drive AD9236. And I want to do x10 attenuation at the same time. I've some guestions:

    1. The ADA4932-1 gives Figure 39, "Open-Loop Gain and Phase vs. Frequency", The phase margin is aboult 45 degree, so…
  • RE: Some questions of ADA4932-1

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: How to use ADA4932-1 with CM on the input

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,