What is meant by "a long time"? Will it start in tens of microseconds...in milliseconds...in seconds? Is it progressively slower to start up as the die temperature is decreased? Does it ever fail to start below 0 ºC altogether? Does it…
What is meant by "a long time"? Will it start in tens of microseconds...in milliseconds...in seconds? Is it progressively slower to start up as the die temperature is decreased? Does it ever fail to start below 0 ºC altogether? Does it…
Hi ADI,
We need an ADC setup to sample a single-ended IF signal. We are considering the AD9635 as the ADC with the recommended ADA4927 as driver and to perform the a single-ended to differential conversion.
The IF signal has beat frequencies down to 1…
hi Gauzz
is there any update on this subject?
what possible issues we may expect using the Vocm at lower voltage?
performance degradation ?
damage the part?
oscillations?
Thanks for your reply
Hi Ozaku,
ADA4860 Theta JC is 48.2C/W. I' have emailed the contact person for Theta JC of ADA4927 and will get back to you.
Regards,
Kristine
The LTC2185 is a 125Msps 16-bit ADC with excellent noise and linearity performance while only consuming 185mW per channel. It is ideal for demanding low power applications that require excellent AC performance. A high performance ADC like the LTC2185…
Hello, I have a question about this feature, in the data sheet says:
The power-down feature can reduce power consumption when a particular device is not in use and does not place the output in a high-Z state when asserted. The ADA4927 is generally enabled…