I'm looking for a single-ended to differential amplifier which can be powered by a single 5 V supply. I.E. Vs+ = 5.0 V, Vs- = 0V.
The ADA4922-1 fits the bill otherwise, and we already use it in some products.
The datasheet advises a supply range…
I'm looking for a single-ended to differential amplifier which can be powered by a single 5 V supply. I.E. Vs+ = 5.0 V, Vs- = 0V.
The ADA4922-1 fits the bill otherwise, and we already use it in some products.
The datasheet advises a supply range…
Dear Supporter,
I have a question about ADA4922-1. Is the Exposed Paddle of ADA4922-1 connected to GND or just a copper plane?
thanks!
Br,
Wayne
Hi All,
I am working one of my project called 8 Channel Receiver.
In this project, I have 8 Channel of differential Analog input.
I will get the all the 8 Channel input from external source with the range of 10Vpp as Max .
I have mentioned my design block…
Hi,
In our system (industry electronics) we use the ADA4922-1 to convert a single-ended signal to a differential signal (a short twisted pair cable will be connected). The issue is that the ADA 4922 gets quite hot, even in steady state condition (when…
Hi
I am using ADA4922-1 to convert a single ended square wave of 1 KHz frequency from single ended to differential. The input square wave have an arbitrary DC offset. In order to remove the DC offset i am using a high pass filter between signal source…
Hi,
I'm designing an AFE for 100 Hz to 5 MHz bandwidth input signal. ADC is 18-bit 15 MSPS SAR with differential input 8.192 Vpp. I have completed my signal amplifying & conditioning circuitry, the only thing that now concerns me is the ADC driver. I…
Hi,
I downloaded ada4922.cir from this page http://www.analog.com/en/design-center/simulation-models/spice-models.html
however it seems that there is an additionnal "Feedback" pin that does not exist in the datasheet.
I believe that the subject…
Hi,
I'd like to know about ADA492201ACP-EBZ. Is there a document of ADA4922-1ACP-EBZ? Is this board same with EVAL-FDA-1CPZ-16? Is there a device on board?