• ADA4897-1, ADA4897-2, ADA4896-2 Maximum Operating Voltage Range

    Will the ADA4897-1 run off a single +5V or +12V Supply Range ?

     

    On pages 4-5 of the data sheet you will find the operating parameters for +5V
    supply range. According to the data sheets, the ADA4897 has a normal operating
    voltage range…
  • RE: OP284 and ADA4897-1 and maximum PCB driving distance

    Hi,

    I would think of additional parasitics in your intended case.
    And this is equivalent of driving more capacitive loads.
    There are several ways of stabilizing your circuit in such case. 
    One is the use of the snubber circuit as also stated on page 18 of…

  • ADA4897: power dissipation calculation

    I have a question about the power dissipation calculation in the ADA4897-1
    datasheet..
    In the “MAXIMUM POWER DISSIPATION” section, there’s the following formula on
    power dissipation. Would you like to explain the definition of “Total Drive…
  • ADA4897 electromigration limits

    Hello,

    Assuming operation well within the power dissipation budget of the device,

    is there a limit on the maximum continuous output current the ADA4897 due to electromigration ? 

    Thank you.

  • ADA4897 electromigration limits

    Hello,

    Assuming operation well within the power dissipation budget of the device,

    is there a limit on the maximum continuous output current the ADA4897 due to electromigration ? 

    Thank you.

  • ADA4896-2\ADA4897-1\ADA4897-2

    请问这三款除了引脚不一样,集成运放数量不一样,4897带了使能端之外,4896与4897的性能是否一致?

  • RE: oscillations in ada4897-1 o/p

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: unity gain amplifier using ada4897-1

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,