• Data Sheet

    Hi.
    In Data Sheet ADA4895-1/ADA4895-2 recorded "POWER SUPPLY Operating Range 3 to 10 V".
    Can i connect power +Vs = +10 V and -Vs = -10 V?

    Thanks,
    Anatolii.

  • Protecting the inputs of the ADA4895-1

    The ADA4895-1 datasheet lists the maximum differential input voltage to +/-0.7V and that the differential current should be limited to 10mA. In the non-inverting mode for a gain of 10x the recommended resistors are Rfb = 226, Rg = 25.5. If the input can…

  • ADA4895-1 output noise

    I would like a sanity check on my noise calculation and the actual result and any other comments.

    Two ADA4895-1 op-amps in series each with a non-inverting gain of 10x. Rf = 226 ohms. Rg = 25.1 ohms, Rs = 51 ohms.

    They are followed by an AD8021 with…

  • ADA4895-1易坏

    使用ADA4895-1ARJZ时,负载约1k欧,反向放大,系统电源±6V,正负电均串联51欧(150欧)后给运放供电。经常发现器件损坏,而且是运放电源被拉至±1.2~±2V左右,而正常工作时运放电源约±5.4V。

    请问容易坏的原因是什么,改进方法除了单独用±5V还有吗?

  • ADA4895-1的问题

    问题描述:

    1、批次1917的芯片都不能用。

    TEST2的波形图如下所示。在超声波信号到来的一段时间(将近33us内),波形是一条直线。33us后,噪声陡增。或者不放大超声波信号。

    2、老的批次基本可以用。

    请问这种现象是因为芯片的原因还是使用的原因造成的?

  • ada4895-1的问题

    原理图如上图所示。

    问题描述:

    1、批次1917的芯片都不能用。

    TEST2的波形图如下所示。在超声波信号到来的一段时间(将近33us内),波形是一条直线。33us后,噪声陡增。或者不放大超声波信号。

    2、老的批次基本可以用。

    请问这种现象是因为芯片的原因还是使用的原因造成的?

  • RE: 26M 1.0V 幅度放大到1.8V

    可以参考一下ADA4895-1 或者 ADA4897-1  ADA4800   ADA4891-1

  • RE: Driving AD9240

    I would like to be able to limit the bandwidth of the ADA4895-1 op-amp. Is there a limit to how large the feedback capacitor can be used on an op-amp that is not unity gain stable? For example using the ADA4895-1, minimum stable gain of 10x, could a feedback…

  • RE: ADA4895-1运放使用

    建议对输入信号源进行衰减处理,使最大信号输入时不至于使芯片饱和。

  • RE: ADA4895-1/2 Data sheet Correction

    Hi Srivatsa,

    Thanks for pointing that out. We'll be working on this.

    Regards,

    Phil