• Operation Amplifier for video-ADA4891-1

    Hi,

    I'm using the ADA4891-1 in a non inverting application - With amplification of 2.

    I'm using VS=3.3V , RG&RF = 604 Ohm, Input resistor-Rt=200 Ohm, I have 100n and 10u Capacitors betweren Vs and Gnd, Input Voltage=1V, output Voltage=Ringing!!…

  • Can the ADA4891-1 be used as a unity gain buffer?

    I was wondering if the ADA4891-1 can be used as a unity gain buffer?  I have a unity gain stable amp on my PCA already but for consolidation of parts and for operating temperature range, I would like use an existing amp I have on my board, the ADA4891-1…

  • RE: Problem  voltage follower AD8548 & ADA4891

    Hi,

    The AD8548 should work smoothly on your case since it is rail-to-rail input/output amplifier while the ADA4891 has an input which is limited to +Vs - 0.8V and that is 4.2V in your case.

    Considering you have a PCB, layout must be taken care to minimize…

  • About ADA4891 LTSpice Model

    Hi,

    I would like to use ADA4891.

    So, I simulated using LTSpice, but the + side of the output voltage will saturate halfway.

    This IC should be a product of Rail to Rail.
    Is the contents of this model correct?

    Best Regards

    Yuya

  • Using ADA4891 for Sample and hold circuit

    Hi ,

    We are using ADA4891 for sample and hold circuit , but would like to know if the Amplifier be stable when the capacitor drains of the

    charge leaving the input similar to that of Floating state.

    We are using a switch before the capacitor connected…

  • ADA4891-1W schematic review at ADV7393 DAC output

    ADA4891-1W schematic review at ADV7393 DAC output by Steven.yang@analog.com

    Hi

    As we discussed, customer would like to apply video buffer amp for 720p YPbPr at ADV7393 output.

    I draw the schematic and the configuration as well in attached file.

    ADA4891…

  • ADA4891-1WARJZ-R7 about storage temperature and Tjmax

    Hello,

    Is storage temperature of ADA4891-1WARJZ-R7 (Qualified for Automotive Applications) −65°C to +125°C ?

    Is Tjmax 125°C ( or 150°C ) ?

    Thanks,

  • ADA4891 Output circuit design (resistor RG design value)

    Hi,

    I am making an experimental circuit and looking at the characteristics.

    I have a question, please let me know.

    The circuit of several hundred channels is switched by the multiplexer.
    The received signal is switched by the following circuit and output…

  • Using ADA4891 as SE to Diff amplifier from Piezo sensor

    Hi

    Is the ADA4891-2 a good candidate to create a SE to Diff amplifier to be used as amplification stage of piezo sensor?

    Currently

  • Is there a Spice model specifically for ADA4891-3 including the output disable pins?

    Hi,

    I'd like to simulate a circuit using the output disable capability of ADA4891-3, but I couldn't find a spice model which includes the output disable pins. Is there one available?

    If so, how can I download it? Can I use it with LTspice?