• ADA4862-3 Disable characteristics

    Hello,

    i miss the disable characteristics from the ADA4862-3 like it is mention in the AD8013 datasheet .

    It crosstalk and it off isolation is very important.

    Can you please publish this information? I need it for a video Board.

    thank u.

  • What is output of ADA4862 in power down?

    Is the output of the ADA4862-3 suitable for video mux applications? (i.e. high impedance when in shutdown)

    In either case what does the impedance of the output look like when in shut down.?

  • what is diffrence between AD4862 and ADA4862, why it does not show datasheet for AD4862 now

    few days back i had found the datasheet for AD4862 with application circuit of active low pass filter 27mhz,23db gain.....what know i am trying to find same AD4862 datasheet again on google, it disappear and results show ADA4862, how it happens

  • 3-Phase 4-wire in to 3-Phase 3 Wire

    How to give input connections to ADE7878 for 3-Phase 4 wire in to 3-PH 3 Wire?

  • what does the "-3" on the brand of ADV7390/1/2/3 and ADV7340/1/2/3 indicate?


    The latest revision of the encoder has the -3 version branded on it's package. The revision code of the encoder can be read back from register 0xBB bits 7:6. 01B indicates the latest revision.

    Further information on the change made to this version…

  • ADE7880 - 3 phase 3 wire delta configuration

    Hi,

    As per the ADE7880 datasheet pg. 43, in three phase three wire delta configuration, Phase B active, reactive and apparent powers are 0.

    So, I would like to know if there is a way to find out the Phase B power data in three wire delta configuration…

  • Output impedance of the LTC6957-3

    Hello,

    I'm trying to match the output impedance of the LTC6957-3 to a 50 Ohm transmission line. In the datasheet of the LTC6957 I didn't found any information regarding the output impedance of the -3/4 variant of the chip. In the datasheet of the evaluation…

  • RE: ADRV9009-ZU11EG Multi-SOM: 3 SOMs delayed from other 3

    Probed all the outputs on the eval board and it appears CLKOUT1,2,4,7,8,11,12 are 180deg out of phase from CLKOUT0,3,5,6,9,10,13 in CMOS mode. Please use only the following outputs as SYNC: CLKOUT0,3,5,6,9,10 and 13

     Added a note about this issue here.

    Thanks…

  • ADAU1467 booting 3 x AD1937 codec's

    Hi there,

    I'm working on a design with a central ADAU1467 DSP connected to 3 x AD1937 codecs so I can have 4 x balanced audio (mic/line) inputs and 24 balanced audio outputs.  I'm at the stage of considering the control.  I like how on the EVAL…

  • RE: ADF4356 Vs ADF4355-3

    Hi,

    Unfortunately, VCO supply is 5 V for ADF4356.

    Kudret