How to give input connections to ADE7878 for 3-Phase 4 wire in to 3-PH 3 Wire?
How to give input connections to ADE7878 for 3-Phase 4 wire in to 3-PH 3 Wire?
The latest revision of the encoder has the -3 version branded on it's package. The revision code of the encoder can be read back from register 0xBB bits 7:6. 01B indicates the latest revision.
Further information on the change made to this version…
Hello,
in the automotive Part List https://www.analog.com/media/en/news-marketing-collateral/product-selection-guide/arpl.pdf
is an LT4356HMS-3#WTRPBF part number listed. I have a problem to find it by any known distributors.
My intention to use an automotive…
Hi,
As per the ADE7880 datasheet pg. 43, in three phase three wire delta configuration, Phase B active, reactive and apparent powers are 0.
So, I would like to know if there is a way to find out the Phase B power data in three wire delta configuration…
Could you please suggest a analog pfc controller for 3 wire 3 phase, 115Vac, 380-665Hz, 380Vout, 800W, min 0,95 power factor? I couldnt find vienna rectifier example or application note at Analog device. My second alternative is 3 phase boost topology…
最近使用ADE9078的三相電能計量, 遇到以下的問題.
問題介紹:
1. 規格書有提到, 計算總功耗(有功, 無功和視在), 須將A相和C相的貢獻相加,
而我運算的結果, 只有"有功"的算完的數值是正確的, 其餘無功以及視在的數值有落差.
硬體介紹:
三相是採用3線Delta, B相接地. 使用EVAL-ADE9078EBZ開發板+EVAL-SDP-CB1Z.
電流部分使用CT(600:1)
參數設定:
VCONSEL設為1, ICONSEL設為0,
…Hi there
Has anybody successfully used multiple FMCOMMS2/3 on a single host board?
Need to get 2 boards (4 channels) working on a single Zc706 under LINUX!
Would appreciate any help in getting FMCOMMS2/3 to work on FMC-HPC under LINUX.
Regards
s…
Hi,
We are using ADP5054 in our design.We need to derive 5.5V with 1A load current from Channel 3 of ADP5054.
I gave this inputs in ADP505x_Buck designer tool and tool suggests to use 12uH SD43-123MLB. Is it fine to go ahead with this inductor MPN?
T…
Hello,
Can we measure a 3 phase system and a 3 single-phase by same circuit using ADE9000 or ADE9078? Off course the meassurement points of the 3 phase system and the 3 single-phase system are different. If no, could you please advise me the connection in…
Hello
I use ADE7880 to analyze total harmonic distortion(THD) in 3 phae 3-wired(Delta connection)
It's OK in ITHD each phase,the value is what I expect
But the value of VTHD is unexpected(each phase), VTHD value is totally different from testing…