• RE: ADA4853 DISABLE Pin

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • ADA4853/ADA4430 "disable" pin

    Hey,

     We have both ADA4853-1 and ADA4430-1 on our board.

    in some scenario it can get a 3.3V in the "disable" pin while no voltage applied to the supply (Vs).There are no details in the datasheet (in the A.M.R section ) referes to this case.

  • RE: Is output High-Z when disable? ADA4851-1

    Hi Jay

    Thank you very much for your support.

    Sorry for confusing you.

    Your information is very helpful for me.

    I would like to know about ADA4851-1,especially.

    But I understood that ADA4853 is able to tie the outputs.

    Regards

    Moto

  • [征文] IN118的基准源用AD的芯片,上面写着D6B,困饶我很久了 AD5312


    这个芯片(AD9833)的名字我猜的,可忽略看,如果是这个芯片,左看右看也不知是干吗呢?

  • ADI芯片辨识、型号查找

    看看截图:

  • AD8324, problems

    Hello,

    I'm building a board with a DSP. The DSP does a FFT on a analog signal. The signal is given a offset and we amplified with a ADA4853-1.

    Then the Signal goes to the AD8324.

    The AD8324 is set in single-ended. The Signal goes to the ADC on…

  • TAGS LIST: Audio

    AD8024
    AD8509
    AD8511
    AD8531
    AD8532
    AD8534
    AD8565
    AD8566
    AD8567
    AD8614
    AD8644
    ADD8504
    ADD8710
    AD8519
    ADSY8401
    AD8529
    AD1870
    AD1871
    AD1877
    AD1974
    ADAU1977
    ADAU1978
    ADAU1979
    ADAU7002
    SSM2602
    SSM26…
  • RE: 3-Phase 4-wire in to 3-Phase 3 Wire

    Good Afternoon

    The ADE7878 can be configured to accept multiple different configurations including 3 phase 4 wire and 3 phase 3 wire wye and delta.  Our FAQ:  AN-639 that is available on our website has detailed diagrams of each connection on pages 12…

  • Are there dual op amps (opamps) with power down / enable / disable function ?

    Are there dual opamp with disable function available?

     

    ADA4895-2:  1 nV/√Hz, Low Power,G≥10 Stable Rail-to-Rail Output Amplifier
     
    http://www.analog.com/en/high-speed-op-amps/high-speed-rail-to-rail-amplifiers/a
    da4895-2/products/product…