Can this pin be left floating with the result that the amplifier is in an enabled state?
Can this pin be left floating with the result that the amplifier is in an enabled state?
Hey,
We have both ADA4853-1 and ADA4430-1 on our board.
in some scenario it can get a 3.3V in the "disable" pin while no voltage applied to the supply (Vs).There are no details in the datasheet (in the A.M.R section ) referes to this case.
…How to give input connections to ADE7878 for 3-Phase 4 wire in to 3-PH 3 Wire?
The latest revision of the encoder has the -3 version branded on it's package. The revision code of the encoder can be read back from register 0xBB bits 7:6. 01B indicates the latest revision.
Further information on the change made to this version…
Hello,
in the automotive Part List https://www.analog.com/media/en/news-marketing-collateral/product-selection-guide/arpl.pdf
is an LT4356HMS-3#WTRPBF part number listed. I have a problem to find it by any known distributors.
My intention to use an automotive…
Hi,
As per the ADE7880 datasheet pg. 43, in three phase three wire delta configuration, Phase B active, reactive and apparent powers are 0.
So, I would like to know if there is a way to find out the Phase B power data in three wire delta configuration…
Could you please suggest a analog pfc controller for 3 wire 3 phase, 115Vac, 380-665Hz, 380Vout, 800W, min 0,95 power factor? I couldnt find vienna rectifier example or application note at Analog device. My second alternative is 3 phase boost topology…
最近使用ADE9078的三相電能計量, 遇到以下的問題.
問題介紹:
1. 規格書有提到, 計算總功耗(有功, 無功和視在), 須將A相和C相的貢獻相加,
而我運算的結果, 只有"有功"的算完的數值是正確的, 其餘無功以及視在的數值有落差.
硬體介紹:
三相是採用3線Delta, B相接地. 使用EVAL-ADE9078EBZ開發板+EVAL-SDP-CB1Z.
電流部分使用CT(600:1)
參數設定:
VCONSEL設為1, ICONSEL設為0,
…Hi there
Has anybody successfully used multiple FMCOMMS2/3 on a single host board?
Need to get 2 boards (4 channels) working on a single Zc706 under LINUX!
Would appreciate any help in getting FMCOMMS2/3 to work on FMC-HPC under LINUX.
Regards
s…
Hi,
We are using ADP5054 in our design.We need to derive 5.5V with 1A load current from Channel 3 of ADP5054.
I gave this inputs in ADP505x_Buck designer tool and tool suggests to use 12uH SD43-123MLB. Is it fine to go ahead with this inductor MPN?
T…