• ADA4853/ADA4430 "disable" pin

    Hey,

     We have both ADA4853-1 and ADA4430-1 on our board.

    in some scenario it can get a 3.3V in the "disable" pin while no voltage applied to the supply (Vs).There are no details in the datasheet (in the A.M.R section ) referes to this case.

  • RE: ADA4853 DISABLE Pin

    Hey,

     We have both ADA4853-1 and ADA4430-1 on our board.

    in some scenario it can get a 3.3V in the "disable" pin while no voltage applied to the supply (Vin).There is no details in the datasheet (in the A.M.R section ) referes to this case.

  • .file_attr 1="1";

    Building a project imported from CCES 1.1.0 to 2.3.0 I get this error:

    [Error ea5004] "C:\Users\G\AppData\Local\Temp\acc3554de5a000\acc3554de5a001.s":659 Syntax Error in :
    .file_attr 1="1";
    syntax error is at or near text '1'.…

  • AD9523-1  Can I precisely adjust output clock frequency with AD9523-1 (EVAL-AD9523-1)?

    Greetings!

    I would like to inquire if it is possible to achieve precise frequency control with EVALZ - AD9531-1? I'm interested in generating a clock signal that is a multiple of femtosecond laser output pulse rate, which can be something close to 80…

  • Arduino UNO and ADXL345 getting 0 0 0 OR -1 -1 -1 outputs with SPI communication

    I have EVAL-ADXL345Z evaluation board from Analog Device hooked up to the Arduino UNO R3, the code complies and runs fine. At first I could still get…

  • RE: Can't get data ADC data to be in [-1, 1) range on EZ-KIT SC589

    Hello,

    We have tested the attached project and it works fine in SC-589 Ezkit.

    If possible, please try it in ezkit if you have.

    Distorted audio mostly caused by Sync issues, Buffer Size, Word length, etc. Please check those areas too.

    Please try and let…

  • AD4110-1 SPI Communication Issues

    Dear Sir or Madam,

    my name is Tristan Strahler and I am part of CURE Mannheim and we are currently evaluating the AD4110-1 AFE for usage in our new PLC systems. The analog functionality of the device exceeded our expectations so we opted to develop a…

  • ADATE305 VDDO_0/1, VSSO_0/1 termination

    Hello,

    In case that VDDO_0 (pin 83), VDDO_1 (pin 93), VSSO_0 (pin 81) and VSSO_1 (pin 95) is unused, what termination is required?

    Best Regards,

  • AD0162-FMCC-EBZ : Could not connect Subclass 1 mode

    Hello,

    I am trying to connect AD9162-FMCC-EBZ and ADS7-V2EBZ by subclass 1 but I could not connect link.
    Subclass 0 mode is ok.

    I used single tone generation which is described in UG-1526 with subclass 1.
    The setup is follows.



    When apply this parameters, spectrum…

  • RE: dev/mem returns -1

    this is libc/glibc specific

    i am not sure this forum is meant for basic libc learning;

    man7.org/.../open.2.html

    RETURN VALUE         top

           open(), openat(), and creat() return the new file descriptor (a
           nonnegative integer), or -1 if an error…