Hello,
One of my customer used below parts in his design-
1- Video Decoder IC ADV7181C
2- Difference amplifier ADA4830-2
please help to review the schemetic.
thanks!
Nikhil Rastogi
I am having a layout from one of my customer having parts ADV7181C and Difference amplifier ADA4830-2.
Customer is violating some recommendation related to placement of ADV7181C relative to graphics VGA connector in this.
Please advise how…
Dear Analog,
Could you please provide the spice model for ADA4830-1? I want to simulate CN-0273 using different first stage op-amp, and I also want to test some ADC driver scheme using dual ADA4830 or ADA4830-2.
Thanks!
Thanks for providing the spice model of both ADA4433-1 and the ADA4830(-1).
I'm trying to design a DC coupled differential transmission system using the ADA4433-1 and the ADA4830.
The overall gain from input (ADA4433-1) to output (ADA4830…
Hi,..I'm using difference amp ADA4830-1 in conjunction with decoder ADV7180 (Circuit Note CN-0263), to receive a CBVS video signal. My question has to do with the ADA4830 input trace geometry on my circuit board. Given that I'll be connecting the…
My JPEG saga continue...
I am using a BF561 single core to compress a 640x480 YUV 4:2:2 image into JPEG format, employing the ADI JPEG Library tools. I am getting very poor performance compared with the reference results from the Spec Sheet. The Spec…
Hello Dave,
I am facing problems with replies to your answer, so I am oppening a new dicussion with the same title.
Please clarify your answer regarding STANAG support:
2) As I understand it, this is the same as RS-343A/EIA-343A and none of our parts…
I installed 2x LTC6811-2 and then 1x LTC6804-2 on the same board and I don't have any voltage reference output at anytime. The functional diagram in the datasheets shows that VREF1 should be always present as it's generated from V+. VREF2 is not…
I am using the ADM1176-2 (latching) part on a new PCB design. I am wondering if setting the SWOFF bit over I2C can reset the latch state the same as toggling the ON pin? The datasheet isn't entirely clear on this aspect--on Page 16 Table 11, it states…
Hi,
I am looking to use the AD7175-2 with an external 5V reference to sample a unipolar differential signal (0 to 5V range); however I was concerned with possible resolution loss compared to bipolar operation (-2.5V to 2.5V range), as some of the other…