• Differential video transmission with ADA4433-1 and ADA4830-1

    Hello,


    Thanks for providing the spice model of both ADA4433-1 and the ADA4830(-1).

    I'm trying to design a DC coupled differential transmission system using the ADA4433-1 and the ADA4830.

    The overall gain from input (ADA4433-1) to output (ADA4830…

  • ADA4830-1 in pseudo-differential mode... input trace geometry?

    Hi,..I'm using difference amp ADA4830-1 in conjunction with decoder ADV7180 (Circuit Note CN-0263), to receive a CBVS video signal.  My question has to do with the ADA4830 input trace geometry on my circuit board.  Given that I'll be connecting the…

  • Request the spice model of ADA4830

    Dear Analog,

    Could you please provide the spice model for ADA4830-1? I want to simulate CN-0273 using different first stage op-amp, and I also want to test some ADC driver scheme using dual ADA4830 or ADA4830-2.

    Thanks!

  • Schemetic review having video decoder ADV7181C and Difference amplifier ADA4830-2

    Hello,

    One of my customer used below parts in his design-

    1- Video Decoder IC ADV7181C

    2- Difference amplifier ADA4830-2

    please help to review the schemetic.

    thanks!

    Nikhil Rastogi

  • layout review having video decoder ADV7181C and Difference amplifier ADA4830-2

    Hello,

    I am having a layout from one of my customer having parts ADV7181C and Difference amplifier ADA4830-2.

    Customer is violating some recommendation related to placement of ADV7181C relative to graphics VGA connector in this.

    Please advise how…

  • .file_attr 1="1";

    Building a project imported from CCES 1.1.0 to 2.3.0 I get this error:

    [Error ea5004] "C:\Users\G\AppData\Local\Temp\acc3554de5a000\acc3554de5a001.s":659 Syntax Error in :
    .file_attr 1="1";
    syntax error is at or near text '1'.…

  • AD9523-1  Can I precisely adjust output clock frequency with AD9523-1 (EVAL-AD9523-1)?

    Greetings!

    I would like to inquire if it is possible to achieve precise frequency control with EVALZ - AD9531-1? I'm interested in generating a clock signal that is a multiple of femtosecond laser output pulse rate, which can be something close to 80…

  • Arduino UNO and ADXL345 getting 0 0 0 OR -1 -1 -1 outputs with SPI communication

    I have EVAL-ADXL345Z evaluation board from Analog Device hooked up to the Arduino UNO R3, the code complies and runs fine. At first I could still get…

  • ADATE305 VDDO_0/1, VSSO_0/1 termination

    Hello,

    In case that VDDO_0 (pin 83), VDDO_1 (pin 93), VSSO_0 (pin 81) and VSSO_1 (pin 95) is unused, what termination is required?

    Best Regards,